cancel
Showing results for 
Search instead for 
Did you mean: 

Problem using TIM3 on DMA1 on STM32G030J6

DRenz.1
Associate II

Dear to All,

I have a boar with STM32G030J6 and I want use the TIM3 as PWM output (on PB0->TIM3_CH3) using DMA1 channel 3 to transfer data from RAM memory to TIM3_CCR3 register. The problem is that DMA never trigger the interrupt!

Here the code:

// Setup Pin PB0 in PWM (TIM3_CH3)

RCC->IOPENR = 0x0000002F;

GPIOB->MODER |= 0x00000003;

GPIOB->OSPEEDR |= 0x00000003;

GPIOB->AFR[0] &= ~0x0000000F; // Reset Alternate Function AF1

GPIOB->AFR[0] |= 0x00000001; // Alternate Function AF1 

// Setup TIM3 per PWM su pi PB0 con DMA

RCC->APBENR1 |= 0x00000002;

TIM3->CR1 = 0x00000000;

TIM3->CR2 = 0;

TIM3->ARR = 0x0000003D;

TIM3->DIER = 0x00000900;

TIM3->EGR =  0;

TIM3->PSC = 0x00000005;

TIM3->SR = 0;

TIM3->CCR3 = 0x0015;

TIM3->CCMR2 = 0x0060;

TIM3->CCER = 0x00000300;

TIM3->CR1 |= 0x00000001; 

//DMA

RCC->AHBENR |= 0x00000003;

DMA1_Channel3->CNDTR = 10;

DMA1_Channel3->CPAR = 0x4000043C;

DMA1_Channel3->CMAR = (uint32_t) &ledValues;

DMA1_Channel3->CCR = 0x00003292;

DMA1_Channel3->CCR |= 0x00000001;

NVIC->ISER[0] = 0x00000400; // int 10

The interrupt on "void DMA1_Channel2_3_IRQHandler(void) " never trigger!

Why? Whats wrong?

Thank you in advance,

Davide

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
waclawek.jan
Super User

DMAMUX channel 0 generates trigger for DMA1_Channel1 (the numbering is mismatched). For DMA1_Channel3 you want to set DMAMUX_C2CR.

Also, keep all fields except DMAREQ_ID in DMAMUX_CxCR zero, unless you know exactly what are you doing.

Also note that DMAMUX clock enable in RCC is identical to DMA clock enable, so you have to set it before you change DMAMUX registers.

JW

View solution in original post

4 REPLIES 4
waclawek.jan
Super User

STM32G0xx contain DMAMUX which determines the triggers routing from peripherals to DMA, you have to set it up.

JW

DRenz.1
Associate II

Thank you JW,

I set up the DMAMUX_C0CR register with 0x00080222 value, but nothing new happen!

Davide

waclawek.jan
Super User

DMAMUX channel 0 generates trigger for DMA1_Channel1 (the numbering is mismatched). For DMA1_Channel3 you want to set DMAMUX_C2CR.

Also, keep all fields except DMAREQ_ID in DMAMUX_CxCR zero, unless you know exactly what are you doing.

Also note that DMAMUX clock enable in RCC is identical to DMA clock enable, so you have to set it before you change DMAMUX registers.

JW

DRenz.1
Associate II

Thank you again JW,

the issue is solved, I set up DMAMUX_C2CR.

Now works fine.

Best regards,

Davide