STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Flashing on STM32G070RBT6

Hi,I’m working with an STM32G070RBT6 MCU and trying to flash it over UART. The UART lines are directly connected to an FTDI adapter, which is connected to my PC via USB. The COM ports show up correctly, but when I try flashing through STM32CubeProgra...

Resolved! STM32H745I-DISCO – CAN TXFIFO Buffer Full Issue

Post edited by ST moderator to be inline with the community rules especially with the code sharing. In next time please use </> button to paste your code. Please read this post: How to insert source code. Hi everyone, I am working on Classic CAN comm...

Sumithra by Associate II
  • 2303 Views
  • 17 replies
  • 0 kudos

STM32N6 max power consumption versus GPIOs usage

New question from this thread. Hi @mƎALLEm  I am using STM32N6 Nucleo-144 board. In this board VDDIO is the power supplied at VDD, VBAT. VDDIO2, VDDIO4, and VDDIO5. So this the the power supply which is driving GPIOs. This power is generated by LD390...

GBA by Associate II
  • 681 Views
  • 2 replies
  • 2 kudos

STM32H750 QSPI External Flash Programming Fails

I'm using an STM32H750XBH6 MCU with two external Flash(W25Q256 X2) chips connected via QSPI. I followed the guide (W25Q FLASH Memory || Part 10 || QSPI & External Loader on H750) to create a custom external loader (.stldr) using STM32CubeIDE, and I m...

WayneLI by Associate
  • 796 Views
  • 3 replies
  • 0 kudos