STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32G431RB Internal Temperature Sensor

Hello, I am working on the STM32G431RB Nucleo board, specifically on the internal temperature sensor. I am facing issues in getting accurate readings. For your reference, I have attached: My code implementation An Excel sheet comparing temperature ...

Resolved! Thermistor reading error with ADC1

Post edited by ST moderator to be inline with the community rules especially with the code sharing. 1- In next time please use </> button to paste your code. Please read this post: How to insert source code. 2- Post is not related to CubeIDE usage b...

Resolved! Heartbeat pulse with DAC and Timer

I tried to search the forum so I'm sorry if there is a solution posted to this problem.I have been struggling with creating the pattern inside the image. Every 10 seconds I want a short heartbeat pulse generated by DAC. (DAC goes high, then low).The ...

paintspot_0-1758561651756.png

Resolved! STM32C011DxY, WLCSP12

I have a question about configuring pin D1 for UART1 TX (in conjunction with pin E2, UART1 RX).Pin D1 has the option for PA11, [PA9], PA8Pin E2 has the option for PA12, [PA10], PA71. To use pin D1 for UART1 TX, PA11 must be switched to PA9 (SYSCFG_CF...

ITEC by Associate
  • 430 Views
  • 1 replies
  • 1 kudos

Why STM32G473CBT6 program failed at 0x0800A000?

Hi there,I am using STM32G473CBT6, and work with a bootloader and application.When I set the application address at 0x08008000, everything works well.However, when I change the application address to 0x0800A000, the application download fails, except...

Junde_0-1758590452323.png
Junde by Senior III
  • 454 Views
  • 2 replies
  • 0 kudos