User Activity

I am not able to enter into the shutdown mode, i am using the below configuration, I wanted to use the wakeup pin 1 to wakeup form the shutdown mode , but in this it is not going to shutdown mode as the current consumption is at 112uA, what is the co...
I am not able to enter into the shutdown mode, i am using the below code  int main(void) { HAL_Init(); SystemClock_Config(); MX_GPIO_Init(); MX_RTC_Init(); MX_USART2_UART_Init(); __HAL_RCC_PWR_CLK_ENABLE(); HAL_PWR_EnableWakeUpPin(PWR_...
I am trying to read multiple channels of ADC (like Temperature sensor channel, Vbat channel, Vrefint ...) using the interrupt method, but I am not able to read all the Channel readings , only the readings of first channel is being reflected for all t...