cancel
Showing results for 
Search instead for 
Did you mean: 

Trying to run a blinking LED on STM32H755ZI-Q

William133467
Associate III

Hi,

am new to STM32 and i am trying to configurate my Nucleo but i don't understand my problem i am trying to setup a basic blink code with the basic structure (serial port communication with putty , debugger stlinkv3 and communication between cores but i can manage to ger it right thank you for any help or advises)

my problem is i cant manage to setup a basic ioc files configuration  for my stm32h755zi-q in the stmcubeide 1.18 i have a basic blink code using both core that work but when i try to setup whit other clock parameters configuration i cant manage to start the program (stlink v3 on the bord look like i cant connect)


1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello,

In your project you set the HSE in Crystal/Ceramic Resonator

mALLEm_2-1741250281583.png

 

mALLEm_1-1741250265714.png

While it should be set in Bypass mode:

mALLEm_3-1741250321188.png

With Input frequency set to 8MHz:

mALLEm_4-1741250370136.png

 

From the schematics, there is no external crystal mounted on the board:

mALLEm_0-1741251071682.png

And the frequency is generated by the STLINK MCO.

See this article.

Attached a project where the two LEDs green and red are toggling. Each led is toggling with a core.

Hope that helps.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

19 REPLIES 19
mƎALLEm
ST Employee

Hello,

In your project you set the HSE in Crystal/Ceramic Resonator

mALLEm_2-1741250281583.png

 

mALLEm_1-1741250265714.png

While it should be set in Bypass mode:

mALLEm_3-1741250321188.png

With Input frequency set to 8MHz:

mALLEm_4-1741250370136.png

 

From the schematics, there is no external crystal mounted on the board:

mALLEm_0-1741251071682.png

And the frequency is generated by the STLINK MCO.

See this article.

Attached a project where the two LEDs green and red are toggling. Each led is toggling with a core.

Hope that helps.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
William133467
Associate III

thank you for your help i am still new to this 
i made the changes in the ioc like you told me 

William133467_3-1741251539818.png


i change some multipliers to get 400mhz , 200 and 100

 

William133467_2-1741251485019.png

 

but i get this error when i try to start for infos i use the configs from
" Getting started with projects based on dual-core STM32H7 microcontrollers
in STM32CubeIDE"


William133467_1-1741251400004.png

 

i get this error now like last time 

William133467_0-1741251175587.png


 

William133467
Associate III

William133467_0-1741253946353.png

i think my problem come from this i am trying on hse 8.33 if this work i will "Accept as Solution" in your reply if it works

thank you

 

 

edit
i change the mco output
and got this error

William133467_0-1741254385088.png

 

 

Just updated my previous post to attach a project where the two LEDs green and red are toggling. Each led is toggling with a core.

Hope that helps.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

thank you for the program this help a lot 

do i use the good stlink config?

do i use this

William133467_0-1741257812039.png

or this configuration?

William133467_1-1741257844301.png

 

also do i use your config or the one provided by :
" Getting started with projects based on dual-core STM32H7 microcontrollers
in STM32CubeIDE"
thank you for your help and time

 

 

You need to use this configuration for this board as we set the input frequency in CubeMx to 8Mhz:

mALLEm_0-1741258618751.png

Meanwhile, in your case and to not complicate the things, as an external clock source is not needed (for example CAN or USB usage), you are just toggling a LED, so you can simply use HSI with PLL:

mALLEm_1-1741258866749.png

 

Hope that helps

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Christophe VRIGNAUD
ST Employee

Hello,

There is no HSE crystal on the Nucleo except if you have soldered one.
So just use the default configuration for STLink default configuration as said above => MCO output = HSI/2.

Double core is a bit tricky when you begin. As a first step, try to get your application work with the default configuration as indicated in the application note.

Best regards

William133467
Associate III

thank you for your informations i am trying to setup a good clock that will be use in my project to generate clocks and signals for a CCD sensors as well as gathering data in real live. i am trying to setep the microcontrolers in the best seteup before ading the timers and gpio 

Hello @William133467 ,

Did you test my project? 

Did you succeed the toggling?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.