STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H747-DISCO Core-Lock Problem

Hello,I’m using the STM32H747. When I set the RCC power source to RCC → Power parameters → Supply source = LDO, the core locks up; if I select SMPS, there’s no issue.When I set CM7 to its maximum clock frequency (480 MHz) and CM4 to 240 MHz, the tool...

CKILI.2 by Associate II
  • 1556 Views
  • 3 replies
  • 0 kudos

STM32L562 UART Data Rx packet loss

Hi,I am using USART4 in STM32L562E-DK eval board. with given configuration. In which I am able to transmit the data correctly on TX based on which UART slave device is sending back the 4 bytes ACK and 16 bytes RESPONSE.Using following codevoid HAL_UA...

414D414E_0-1757398146959.png
414D414E by Associate
  • 1012 Views
  • 5 replies
  • 2 kudos

i2s clock issue in stm32h723zg

hello, i hope you are doing good. i am facing an issue in configuring i2s in dev board nucleo-h723zissue i am facing is no clock at i2s2-sck pin.i tries all other i2s port also. i checked clock through logic analyzer .here is my clock configuration: ...

sajidehsan194_0-1757422544161.png sajidehsan194_1-1757422574730.png sajidehsan194_2-1757422636993.png

Resolved! STM32H743VIT6 ADC didn't run

Dear all!i'm handle graduation thesis project: " design driver for PMSM using STM32 base external mode with Matlab simulink"i design hardware as PDF file, all block working without ADC, i try to set up by STM32cubeMX 6.14 but it still can't run, so c...

Bootloader for STM32F746 for firmware and QSPI

Apparently I can not easily update my application firmware for stm32F746 toughGFX app with just one Bin file. I have written a bootloader for an SD card. It loads firmware at 0x08040000. I am not sure I understand everything that is going on here, so...

FJB2069 by Senior
  • 495 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F411 Blackpill + eMMC (Raspikey) + FatFS

Hi,I have a STM32F411CEU6 Blackpill that I'm wanting to interface to an eMMC (Raspikey to be exact via SD/MMC reader) with FATFS. I have confirmed that the connections with the SD/MMC reader are fine with a read/write test to an SD card in a differen...

chasej by Associate II
  • 940 Views
  • 2 replies
  • 2 kudos

Resolved! STM32F303RET Clock Issue

I have a design that I have used in the past but a latest build I am having trouble with the system clock. I am using 8mhz crystal, IOC file HSE is setup to use the crystal. I cannot get the processor to run above 16 Mhz. I have older projects that u...

bradbas by Associate II
  • 893 Views
  • 9 replies
  • 1 kudos

Resolved! H743 FMC SRAM memory fault

I tested FMC speed on F403 and H743. F403 works fine but H743 code will stopped due to memory fault.I set FMC parameter like belowMy plan is to connect stm32 to fpga by using FMC so did this test to check the speed. F407 test succeeded.But H743, the ...

F407.png F407_code.png H743.png H743_code.png
snkparty1 by Associate III
  • 1361 Views
  • 3 replies
  • 1 kudos