STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Can't enable any register in debug mode stm32cubeide

Hello everyoneI have a little problem with stm32cubdeide, when im trying to work in debug mode with the mcu stm32f469nih6 i can't modiffy or add any bit to enable the register RCC->AHB1NER->GPIODEN.I just want to set clock to activate other peripheri...

0693W00000Y6wDLQAZ.jpg
JBece.1 by Associate
  • 1495 Views
  • 3 replies
  • 0 kudos

FDCAN TX fails about half of the time (HAL)

Hello,I've set up FDCAN on my STM32H753. I'm reading the transmissions using both an oscilloscope and an Analog Discovery 2.I'm currently debuggning a loop which transmits the same message over and over again. About half of the times I only get the S...

0693W00000Svdc5QAB.jpg 0693W00000SvdcAQAR.jpg

STM32G0B1 fdcan can't recieve messeages.

I am currently implementing communication between STM32G0B1 and STM32H743 using FDCAN.However, I am unable to receive stably. Sometimes it works, sometimes not.Specifically, the following is happening.(G0B1 Recieve)・Data is actually in Fifo, but no r...

Haru by Associate II
  • 2929 Views
  • 3 replies
  • 1 kudos