STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Use same port to write as well as read

Hello,Currently I am working on a 16-bit parallel interface where I need to write to and read from the same port. For that I am using GPIO_Init LL library every time I do so. Is this the right method? Will the port data also get reset while doing so....

HDesa.1 by Senior
  • 4108 Views
  • 8 replies
  • 0 kudos

The role of AVDD on Nucleo-L476RG

Hi people!I am currently using a Nucleo-L476RG connected to an analog sensor. On the datasheet of the mcu, in the ADC section, I can read "One external reference pin is available on some package, allowing the input voltage range to be independent fro...

0693W00000Y6vAuQAJ.png
mdiro by Associate III
  • 4709 Views
  • 4 replies
  • 1 kudos

Bit levels matter

Anyone seen this? The politically-correctness crap gets to EE...https://www.oshwa.org/a-resolution-to-redefine-spi-signal-names/

Pavel A. by Super User
  • 1732 Views
  • 5 replies
  • 2 kudos

Need help in making USART2 work on STM32F303RE

Hi, I am doing a MOOC for learning STM32 programming, in the UART topic, we are supposed to implement UART. The course follows STM32F4 but I have an STM32F303RE and I tried to adapt it to my board but it is still not showing anything on the serial mo...

SKhan.7 by Associate II
  • 6326 Views
  • 17 replies
  • 0 kudos

So far 2 boards have died and I am uncertain how they failed, is there a chance they could be fixed through software?

I was using a Nucleo F746zg to develop firmware and in the middle of testing after consistently functioning for over an hour, it stopped communicating with the st link and started showing an overcurrent error. After further testing, the voltage regul...

AZeli.1 by Associate II
  • 7188 Views
  • 16 replies
  • 0 kudos