STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Count External Pulses Using Timer

Hi All,First post :beaming_face_with_smiling_eyes: I want to count external pulses with a STM32F105 or STM32F405 using the HAL library. I want the external pulses to increment the timer counter. I want to avoid using interrupts. Instead, I want to re...

Resolved! CANBUS on F0 not able to receive.

I am working with the STM32F072CB device on a custom PCB. Working from this STM32 example.I just want to implement a basic loopback test. However i don't seem to receive any data.HAL_CAN_Init() is called succesfulHAL_CAN_Start() is called succesfulHA...

JWieb by Associate III
  • 1656 Views
  • 2 replies
  • 0 kudos

TIM_DMAError with ErrorCode 1

Hi, I am trying to send WS2812 LED data as PWM signal using DMA. All works on STM32F091/STM32F103, but when I try to do it on STM32F407 sending via DMA fails.My TIM1/DMA/NVIC settings: I am trying to call:HAL_TIM_PWM_Start_DMA(&htim1, TIM_CHANNEL_1, ...

0693W00000Y8pc8QAB.png 0693W00000Y8pcDQAR.jpg 0693W00000Y8pcNQAR.jpg
JBond.1 by Senior II
  • 1536 Views
  • 1 replies
  • 2 kudos

memcpy vs split SPI transfer

Hello,I came across this question while writing a driver and I would like to ask what is your best practice in this regard. So lets say you want to interface with an chip via SPI. To perform any action, a command byte or a sequence of commands is req...

MLang.7 by Associate III
  • 1713 Views
  • 1 replies
  • 0 kudos

STM32F779AIY6 - What if NC pins are connected to GND?

Hello,i just received some custom boards with a STM32F779AIY6 on it.3V3 net and GND net have a short circuit when MCU is soldered, without MCU there is no short circuit.I checked everything, it should be fine.But what i just found was that the datash...