STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Why is my ADC reading zero for values?

My objective is to utilize ADC peripheral for reading analog signals and converting them to digital. I am using the polling method for reading ADC values. When setting up the chip configuration, I am currently using the Nucleo-H743ZI with default set...

0693W00000FCaDFQA1.png 0693W00000FCaDtQAL.png 0693W00000FCYf3QAH.png 0693W00000FCaJSQA1.png
LRive.1 by Associate
  • 5596 Views
  • 4 replies
  • 0 kudos

Variable NOR flash wait-states using the STM32F4's FSMC

Hi all,I'm planning to use an STM32F405 and its FSMC to interface with an external, parallel 16-bit NOR flash chip from Infineon/Cypress.This chip has a read page size of 32 bytes / 16 half-words.When reading a half-word that is located in a page whi...

DashNode by Associate
  • 1135 Views
  • 0 replies
  • 0 kudos

TRGO and Repetition counter? STM32L476

I have a prescaler (20), an ARR of (65535) and a Repetition Counter of 3 on a 20MHz clock ....On the scope it all looks good...Question if I set a timer up to be triggered by the Update Event, will the timer being triggered update on the output I see...

SWenn.1 by Senior III
  • 2542 Views
  • 2 replies
  • 0 kudos

Resolved! In RM0394 Rev 4 page 873/1600 field OCM1 is bits 6:4 which I count as 3 bits. But the description shows the settings as 4 bits with 16 choices.

For example: 1000: is Combined PWM Mode, 1111: is Asymmetric PWM Mode 2. How do you fit 4 bits into 3 bit spaces? Bit 7 is used for OC1CE, and Bit 3 is used for OC1PE so there is no space on either end for the extra bit.

KiptonM by Lead
  • 2782 Views
  • 3 replies
  • 0 kudos