STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

bh1750 sensor i2c poll method working fine but i2c DMA method not working with attached code . will DMA only transfer the value to global variable ?

  #include "newblue_bh1750.h"     I2C_HandleTypeDef *bh1750_i2c; // Handler to I2C interface   bh1750_mode Bh1750_Mode; // Current sensor mode uint8_t Bh1750_Mtreg; // Current MT register value   void BH1750_Init(I2C_HandleTypeDef *hi2c) { bh1...

0693W00000YAVmWQAX.png
MMARI.1 by Senior II
  • 2732 Views
  • 3 replies
  • 0 kudos

12 one time pulse timer ?

Hello !I need to create 12 (separately triggered pulse trains for thristors) one time pulse timers. (one pulse train consists of approx 10 pulses with approx 10us wide) Many stm32s only have 2 or 3 timers with RCR ( one pulse timer with repetition c...

OYoru.1 by Associate II
  • 1000 Views
  • 1 replies
  • 0 kudos

Resolved! DFU STMProgrammer issue

I use CLI for flash F469 and same hex file flashed over SWD without error produce over DFU this. is this know issue ? Seems code is ok after both loads.

0693W00000YAhtuQAD.png
MM..1 by Chief III
  • 1633 Views
  • 2 replies
  • 0 kudos

Resolved! How to remove autogenerated code generated by MxCube?

I have used MxCube to enable an ISR that is triggered from an external GPIO input pin. MxCube enables this ISR from the autogenerated MX_GPIO_Init() function by calling HAL_NVIC_EnableIRQ(EXTI15_10_IRQn); at the very end of this function. I don't wan...

MFolk.1 by Senior
  • 2364 Views
  • 3 replies
  • 0 kudos