STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How do I use timer 7 on an STM32L433 to time an event?

I am trying to use timer7 to give me the number of counts when an event occurs.  I could not get this to work, and wrote some test code to show the issue.This test code should set the initial count to zero, then fill an array with 10 timer values as ...

JMala.3 by Associate III
  • 1554 Views
  • 2 replies
  • 0 kudos

Resolved! SMPS Electrical Specifications

Would you be able to provide electrical specifications for the integrated SMPS of STM32U585CIU? Specifically: power efficiency at different loads, output current capability, switching frequency, etc.Thank you,

ASlep.2 by Associate II
  • 2835 Views
  • 5 replies
  • 0 kudos

STM32U5 FDCAN version

Hello all,we intend to use the STM32U5 in a project that uses CAN FD. I have learned that the initial CAN FD version 1.0 specification from Bosch [1] in 2012 had a bug that prevented the CRC detecting some error types, which led to changes during the...

printf and float

So, I'm having an issue getting the printf() function suite to work with floating point values.First, understand that I am not using STM32CubeIDE. It's a good tool, but I've had too many issues/complications using it. I use a custom Makefile and VSc...

About setting QSPI from ioc

Hi I am testing a STM32H745I-DISCOI am setting QSPI from ioc file by referring to the example code provided by STBelow is the example qspi configuration code​  QSPIHandle.Instance = QUADSPI;​  /* QSPI initialization */  /* ClockPrescaler set to...

0693W00000YAh2kQAD.png

Understanding interrupt latency in the Cortex M0

Hello,Currently, I use STM32F030K6. I programmed timer 3 to have a period of 1μs, but I noticed at the oscilloscope that my signal has a delay of 16μs, so I searched the datasheet and I found this:I wonder if it is at each interrupt?, and how to deal...

0693W00000YAfzLQAT.png
AKENZ.1 by Associate II
  • 4036 Views
  • 5 replies
  • 0 kudos

STM32CubeProgrammer - no st-link detected (win7)

ST-LINK V2 works fine with STM32 ST-LINK Utility and STM32CubeIDE, but ST-LINK V2 doesn't work with STM32CubeProgrammer.Any idea why this might be? I have tried various USB ports and various USB to mini USB cables. I am using original programmer and ...

Resolved! STM32 L412 Timer interrupt not working

I am using STM32L412 microcontroller and doing baremetal programming for timer interrupt. I am using Timer 6 and base clock of 4MHZ is used as HCLK. However my interrupt is not firing below mentioning my code. count variable is also not updatingint m...

SSaiy.1 by Associate III
  • 6419 Views
  • 14 replies
  • 0 kudos

Restart without Register RCC->CSR bits set (STM32F417ZGT6)

Hi there,we have an application which already tracks register RCC->CSR on startup and writes the content to the log files.From time to time, due to (intentionally unfiltered) electrical disturbances in the electronic or external EM pulses, we see the...

Ingmar by Associate II
  • 690 Views
  • 0 replies
  • 0 kudos