STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to read Data with I2C from 3 Byte register?

Hello, I am new to STM32 so I am currently try get the basic done. I want to receive like written in the title, the temperature data from the BMP388 sensor. Therefore I looked up the Datasheet and found out that I need following registers.#define SLA...

Y-E-Quit by Associate
  • 3097 Views
  • 5 replies
  • 0 kudos

Resolved! STM32F746IGT - Cannot trigger ADC conversion with Timer 4

Hello,I'm working on hobby project using STM32F746IGT. I wrote ADC init sequence but cannot get it working properly. Timer 4 reloads at given period and It's interrupt is called properly. ADC starts conversion after setting SWSTART bit manually but I...

RZieb by Associate II
  • 5541 Views
  • 11 replies
  • 0 kudos

Using indications instead of notifications with BLE

Hello,I have a question regarding implementation of BLE on proteus and nucleo boards.I am struggling to understand how confirmation of indication is processed by the server (and also how does client provide this confirmation). There doesn't seem to b...

NRist.1 by Associate
  • 1196 Views
  • 0 replies
  • 0 kudos

Hex or bin with multi-firmware

My solution have more than one project, each project program in different address. exp: bootloader(0x08000000, 64K) application(0x08010000. 448K).How can create an hex or bin with these two ?

Lwang1 by Associate II
  • 1360 Views
  • 2 replies
  • 0 kudos

connect two stm32 board using uart

Hi, may I know how to connect two stm32 board using uart?Im using nucleo g071rb to transmit the data to STM32H750-DK. So basically i just want to try simple application using serial but it not successful.so what i want to do Nucleo G071 transmit data...

0693W00000YAQ7EQAX.png 0693W00000YAQ8CQAX.png 0693W00000YAQ7iQAH.png 0693W00000YAQ7YQAX.png
Angle by Associate II
  • 9462 Views
  • 5 replies
  • 0 kudos

Waveform Non Pin Timer GPIO STM32F429IGTB

Hi All,I want to generate digital clock/waveform at non timer pin STM32F4219igtb, let say using pin PORTD.5 and synchronize with several GPIOs using DMA. the purposed to drive the multiple HUB75 port.Currently i'm succeed to drive the clock pin using...

Mhida.1 by Associate
  • 1038 Views
  • 0 replies
  • 0 kudos