cancel
Showing results for 
Search instead for 
Did you mean: 

Temperature Sensor Responding Time with STM32Fxx

Texram
Associate III

We have been using STM32F0x, STM32F30x and we read an ADC channel to get the temperature.

we would like to know on-chip Temperature Sensor Responding Time. (How fast does the sensor respond to the temperature change?)

Thanks

David

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
S.Ma
Principal

I guess it measured a junction temperature, so it is nearly immediate, and varies with chip power consumption. Package has thermal inertia, so are the pcb soldering and any heater copper. Maybe considering the internal sensor for ambiant temp measurement should use true external sensor. Did you know smartphones cannot measure ambiant temperature for similar reasons?

Texram
Associate III

Thanks for the comments.

Does STM have the number on 'How fast does the sensor respond to the junction temperature change'?

AScha.3
Super User

response to the junction temperature change is in ms - range, because sensor is also junction on the chip. so if chip gets 1° more hot or cold, you see it on next moment/measurement.

If you feel a post has answered your question, please click "Accept as Solution".
S.Ma
Principal

To be accurate, you measure the instant temperature of a specific point on the rectanglr silicon chip. Intel has several sensors especially in multi core chipsets.