STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Timer triggered DMA doesn't work

I want to sample GPIO state twice per millisecond with DMA.I used TIM16 as basic counter - setting TIM16 CR1 register to 1, ARR to 32000 (half milisecond) and TIM16 DIER register to enable DMA on update (bit 8).Timer is checked to work fine. DMA doe...

WojtekP1 by Associate III
  • 2603 Views
  • 5 replies
  • 0 kudos

Resolved! Does STM32F767ZI support Battery charging detection (BCD)?

Hello team!I am newbie in STM32 world so probably i am missing something but please clarify this for me. I have found conficting informations:Datasheet "DS11532 Rev 7" at p. 47 says "Battery Charging Specification Revision 1.2 support"Reference Manua...

ŁJura.1 by Associate II
  • 1747 Views
  • 2 replies
  • 0 kudos

Are there small packages with OSC-In/Out pins?

Been browsing through the Lxxx and Gxxx STM32 MCUs and found that all variants I checked on hat the OSC-In and OSC-Out pins available only with 48 pin and higher packages.Is this a general rule, or are there MCUs with small package (preferably TSSOP...

b.a. by Associate III
  • 1910 Views
  • 4 replies
  • 0 kudos

Resolved! Debug STM32L072 using ST-LINK/v2?

I am rather new to STM32. Ιn my project, I am using an STM32L072KZU6 and I want to debug the firmware using the ST-LINK/V2-ISOL. I connected both SWDIO and SWDCLK pins to pins 7 and 9 of the ST-LINK/V2-ISOL, along with +3.3 V on pin 1 and ground on p...

0693W00000aINKGQA4.png 0693W00000aINO1QAO.png 0693W00000aINP4QAO.png 0693W00000aINQHQA4.png
GMeta.2 by Associate
  • 2311 Views
  • 2 replies
  • 0 kudos

Wrong ADC values. Why?

Target: STM32L031C6T6editor: SMT32CubeIDE using HALI getting crazy soon. I cannot get this ADC to read correct. I think I missing something important. I googled and googled again and again.I have two voltage on two separate channels (7 & 8). 6.9V and...

Haddock by Associate III
  • 4475 Views
  • 3 replies
  • 1 kudos

Resolved! For STM32G4xx, please clarify role of BFB2 in option bytes

If BLB2=1, hardware maps the System memory to address 0. The bootloader might've remapped it when it detects "valid code" in either bank, but it apparently does not do it, as witnessed by footnote to SYSCFG_MEMRMP.MEM_MODE description:1.When BFB2 bit...