STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STEVAL PROTEUS-1 - Modal analysis using impact hammer

Dear all, I'm trying to evaluate the IIS3DWB sensor using the STEVAL PROTEUS-1. Would it be possible to use the sensor to capture transient vibration e.g. Modal test using an impact hammer? Is there an example script for STEVAL PROTEUS-1, to capture ...

Ravide by Associate
  • 801 Views
  • 0 replies
  • 0 kudos

STM32F030CC Bootloader application stuck at first HAL_Delay

Hi, I am working on STM32F030CC microcontroller, where I am calling an application code from bootloader code. When the code is entering the application, the program is entering into an infinite loop of HAL_Delay(). I found out that by adding "SCB->VT...

JObbu.1 by Associate
  • 1329 Views
  • 1 replies
  • 0 kudos

SRC236/441 libs with Hard FPU support?

I believe all of the audio processing addon libs, (SRC236/SRC441) are built without hardware FPU support. The problem is my entire project was built with hard FPU support. I tried the mixed SW/HW, but that didn't solve the issue and I couldn't build ...

Zaher by Senior II
  • 2497 Views
  • 3 replies
  • 1 kudos

Communication with STEVAL-MKI109V3 kit

I would like to use STEVAL-MKI109V3 with LSM6DSV16x Imu sensor. I have other tools like ESP32 and some sensors that controls autobrake system based on IMU data. I communicate between ESP32 and PC(Python) through BLE. However, if I add STM32F401VE. th...

FKara.3 by Senior
  • 734 Views
  • 0 replies
  • 0 kudos

Resolved! SPI Signal Shape Issue

Hello,I am try to control an external DAC system with the SPI interface. The clock signal shape looks like the attached file. I didn't figure out the meaning of the signal. Yellow is the clock signal and the blue is CS signal.

0693W00000aJE10QAG.jpg
AE104 by Senior
  • 7302 Views
  • 24 replies
  • 0 kudos

Bit Banding issue

I have an issue with using bit banding on stm32U575ZI-Q board when I want to write on it Hard fault is appear what is the problem and How to overcome this issue?

rsoli.1 by Associate II
  • 2468 Views
  • 3 replies
  • 0 kudos