cancel
Showing results for 
Search instead for 
Did you mean: 

Flash read/ writing

AShel.1
Associate III

Hello,

is there a method to read/ write NOR flash on QSPI

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
ChahinezC
Lead

Hello @AShel.1​,

For read/write NOR flash using FMC interface, you can check the examples provided within the STM32Cube_FW.

For instance the one on the STM32L476G-EVAL, you can find it under the "...\STM32Cube_FW_L4_V.XX\Projects\STM32L476G-EVAL\Examples\FMC\FMC_NOR" root.

To get quick technical support on further threads, I advise you to provide detailed description concerning your question/problem, the setup you are working with, etc..

Thank you.

Chahinez.

View solution in original post

4 REPLIES 4

What thread?

The MTP plumbing would presumably go to an underlying file system.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
AShel.1
Associate III

I'm using FMC mechanism

I'm using FMC

ChahinezC
Lead

Hello @AShel.1​,

For read/write NOR flash using FMC interface, you can check the examples provided within the STM32Cube_FW.

For instance the one on the STM32L476G-EVAL, you can find it under the "...\STM32Cube_FW_L4_V.XX\Projects\STM32L476G-EVAL\Examples\FMC\FMC_NOR" root.

To get quick technical support on further threads, I advise you to provide detailed description concerning your question/problem, the setup you are working with, etc..

Thank you.

Chahinez.