STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H747 with ADV7280/TVP5150 unable display image

I’m using an analog camera with a CVBS output connected to an ADV7280/TVP5150, which interfaces with the DCMI on the STM32H747. However, the LCD display is not showing any image. Previously, I used the OV5640 camera, and it worked fine. void CAM_DMA2...

KHowe by Associate II
  • 667 Views
  • 1 replies
  • 0 kudos

Resolved! STM32H757 SWO Debug Error

I get the following error when trying to debug an STM32H757 with SWO enabled. Failed to enable SWV configuration.Failed to execute MI command:-data-write-memory 0x5c003010 x 4 0x77etc...It would seem the debugger (ST-link v2) is not able to read the ...

CWadd_0-1730695812762.png
CWadd by Associate
  • 2811 Views
  • 14 replies
  • 5 kudos

STM32F373 SDADC Offset Error

We want to use the SDADC to measure the temperature of a PT100 sensor. The measurement should have a very high accuracy of +-0.5Kelvin. Therefore, it is important to have a low offset error. The datasheet lists very large values ​​for single-ended mo...

MaxMueth86_0-1759412023795.png MaxMueth86_1-1759412496444.png

Resolved! One Pulse Mode and ICP with one Input Pin

Hi,What I want to implement is to receive the Input Trigger (called Ch1) signal on the rising edge in One Pulse Mode and output a PWM signal through Ch2. At the same time, I want to capture an ICP interrupt on both the rising and falling edges of Ch1...

Space saving power solution for STM32N6

Hello, I'm working on finding the smallest possible power solution for the STM32N6. The reference boards(STM32N6570-DK and STM32N6 Nucleo-144) uses multiple discrete buck converters and LDO to power the N6. It must be possible to do it smaller. From ...

KenH by Associate
  • 719 Views
  • 0 replies
  • 0 kudos