User Activity

Hi, I was hoping to evaluate ethernet connection of my nucleo H755ZI-Q board. It turns out to be more challenging than I initially though. I have tried to follow this example: https://community.st.com/t5/stm32-mcus/how-to-create-a-project-for-stm32h7...
Hi, I would like to evaluated ADC of STM32H745. I would like to have 12bit 5.12MHz dual ADC. According to my understanding, I need to use model STM32H745II in 176 pin UFBGA to obtain ADC performance. Is there any board like nucleo, which can be used ...
From a previous question: https://community.st.com/t5/stm32-mcus-products/stm32h745-dac2-missing/td-p/750749 So I can get two independent analog outputs using STM32H745?
Hi, I would need dual DAC using STM32H745. According to datasheet, it should have two DAC converters. In STM32CubeIDE, I can see only DAC1 with two channels. In the datasheet, I can only see DAC1_OUT1 and DAC1_OUT2 pins, but no DAC2 out pins. Is ther...
Hi,I'm looking for baseband processor for my IQ receiver. I would need dual 12-bit ADC with 5.12MSPS rate. I hope to get data from two ADC to DMA syncronously.I have been looking for STM32H745 for this task. Based on the datasheet, maximum sample rat...