STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 PWM 2 phase

i have a question my friends, i did PWM for 2 Phase, it works correct and good, but after i stop my Timer Master and Slave in order to have Delay, i mean with HAL_ TIM_PWM_STOP, doesn't work my timer slave any more, can you help me about that?Here ar...

HA.5 by Associate III
  • 2266 Views
  • 5 replies
  • 0 kudos

SM32F411, SPI slave without NSS still receives data

Hi,I have configured an SPI as receive-only slave in CubeMX and have set NSS to "Hardware input signal":From logical point of view I now would expect, that there are no SPI data received, as long as NSS stays at high.However, the CubeMX-generated cod...

_legacyfs_online_stmicro_images_0693W00000bjkvVQAQ.png
BSchm.6 by Associate III
  • 2411 Views
  • 4 replies
  • 0 kudos

Resolved! Past Online workshops

Hi all,Does anyone know if I can watch a past Online workshop called 'Easily add intelligence to your products'? I missed the scheduled one on the 4th April and would like to watch it if available.Thanks.

MHarr.8 by Associate II
  • 1553 Views
  • 2 replies
  • 0 kudos

STM32F411RE: EXTI3 interrupt does not work

Hi,when configuring PA0/EXTI0 interrupt in CubeMX, the related code works well: when PA0 pin is toggeled, the ISR is called and following up from this, the code jumps into HAL_GPIO_EXTI_Callback().But when doing the same with PA2/EXTI2 or PA3/EXTI3 t...

_legacyfs_online_stmicro_images_0693W00000bjlAaQAI.png
BSchm.6 by Associate III
  • 903 Views
  • 1 replies
  • 0 kudos

Resolved! STM32U5 and Hyper ram

Hi,​After I configure hospi1->Init.MemoryType = HAL_OSPI_MEMTYPE_HYPERBUS;​If I still want to send a command using CA[47:0] (or DQ[7:0]) and read back data such as device ID, how should I approach this? Is there an example code I can refer to?I am wo...

dchen by Associate II
  • 1969 Views
  • 1 replies
  • 0 kudos

Cant use internal watchdog while using flash

hi I am using stm32l496 and when I use flash the watchdog gives error for some reason. and if for some reason flash works the watchdog always fails.Is there any solution anyone else has faced this issue ?

HZaib.1 by Associate III
  • 1350 Views
  • 2 replies
  • 0 kudos

Cordic Configuration STM32G4

Hello all,I want to use the Cordic accelerator in a STM32G4 and calculate the atan2 from 2 input arguments. Now two questions arise:1) Is there a package for CUBE so I can configure it there? Up to now I only see the activation button.2) If there is ...

Bench by Associate III
  • 3936 Views
  • 4 replies
  • 0 kudos