STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! FIT rates (failure rates) - MTBF/MTTF calculations

Dear ST Technical Support, I am looking for reliability data for the STM32L151 series microcontrollers, including:- FIT rates (failure rates)- MTBF/MTTF calculations - Lifetime expectations- Qualification test results Could you please provide the rel...

zhaowhong by Associate III
  • 617 Views
  • 3 replies
  • 0 kudos

Resolved! STM32H747IGT6 - Extreme Heat

Hi AllHope everyone is well,Im working on a large and expensive project that requires dual core processing, therefore prior to committing to the cost of my project I created a custom dev board  to ensure I can achieve what is required for my project....

SCH_BMS Avinoics 2.0.1v_1-STM32H747IGT6_2025-10-19.png Top Assembly Drawings_page-0001.jpg
Caller89 by Associate
  • 551 Views
  • 3 replies
  • 1 kudos

Resolved! STM32H747BIT6 Not running code

I have been working recently on a board that i have made for a flight computer. But unfortunately, I have encountered some problems while programing the board.The conection to the board works great, and I´m able to upload de code and read it. The Iss...

Resolved! USBX MSC + FileX + NAND Flash - Windows I/O

Hello,I am building and application with a STM32U575 and a 4Gb NAND Flash. What I am trying to achieve now is to upload files from my PC through USB and then used these file within the STM32 using FileX.I already managed to set up FileX and LevelX to...

Pepils by Associate II
  • 13124 Views
  • 10 replies
  • 4 kudos

Resolved! STM32H7S7L8 dual USB

Hi ,I'm working on the STM32H7S7L8-DK and i would like to know if it is possible to use both USB_FS and USB_HS as two separate Virtual-port-com Device mode When I try to do it for one it is impossible in cube MX to do it for the other.Thanks !  

Hamady_1-1760681664387.png
Hamady by Senior
  • 717 Views
  • 8 replies
  • 0 kudos

Resolved! stm32h723zg Clause 45 MDIO

Hi all,i see H7 supports clause 45 MDIO access, but in the HAL library looks not implemented, i see only clause 22.How should i proceed to read/write c45 ? Thanks,angelo

heisenbug by Associate III
  • 3818 Views
  • 13 replies
  • 5 kudos