STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to add Cortex-M33 to TrueSTUDIO ?

I know TrueSTUDIO is tagged as obsolete, but I like to use it.The STM32H5 use Cortex-M33 core, then how to add M33 support?I already upgraded TrueSTUDIO to support GCC 10.3.1 and recent loaders and SVD files. It would be nice to use M33 cores with Tr...

_legacyfs_online_stmicro_images_0693W00000blDmmQAE.png

Resolved! Bit-banged I2S on STM32F103

Hello everybody,I am trying to bit-bang an I2S interface on an STM32F103 at 72MHz using TIM2.Am I way too optimistic to get a 3MHz "clock" out on a pin? The fastest I can seem to get it is at 90kHz.I have set the "prescaler" of TIM2 to "0" and "1".An...

PGild.1 by Associate III
  • 5474 Views
  • 4 replies
  • 0 kudos

STM32F411RE and nrf24l01 module compatability issues

Sir I am doing my final year project and got struck. My project aim is to receive data from the nrf24l01 module which connected with arduino for generating sinewaves this act as TX part. Now in RX part I am using nrf24l01 with STM32f411re and I want ...

RM.7 by Associate
  • 1717 Views
  • 1 replies
  • 0 kudos

NUCLEO 144 board power consumption depends on the link order of the compiled objects in your STM32CubeL4/Projects/NUCLEO-L496ZG/Examples/PWR/PWR_ModesSelection example

When running your PWR_ModeSelection example on a NUCLEO-L496ZG board the current consumption in run range 2, 24MHz depends on the order objects are linked in the executable. When the object_list is in this order:hal/stm32l4xx_hal.ohal/stm32l4xx_hal_...

How to fix a glitch in output PWM from TIM1 of STM32G031xx?

I am using STM32G031 where in my application I have to capture the frequency of Input signal from a sensor and then generate an output PWM with frequency which is twice of input frequency. I am using TIM3 to capture the input signal from sensor and c...

HSing.5 by Associate II
  • 2489 Views
  • 2 replies
  • 0 kudos

Resolved! STM32H5 Comparator always trigger interrupt

Hi. I get a STM32H5 Nucleo board (MB1814) and configured comparator with neccessary settings using CubeIDE and LL library and got next generated piece of code.int main(void)   {   NVIC_SetPriorityGrouping(NVIC_PRIORITYGROUP_3);   SystemClock_Config...

CChen.19 by Associate
  • 3873 Views
  • 1 replies
  • 0 kudos

Reading TIMx->DMAR from unrelated (channel/stream) DMA request

Hello,I was looking for datasheets or specs or any other information from knowledgable people about reading a timer's DMAR register from a DMA request triggered by *another* timer. I was wondering how much reliable this design is, and if I should thi...

tho by Associate
  • 2790 Views
  • 3 replies
  • 0 kudos

Ordering the NUCLEO-H563ZI in connection with the " STM32H5: Ultimate combination of performance, integration and affordability" failed.

Something went wrong when I tried to order the NUCLEO-H563ZI in connection with the " STM32H5: Ultimate combination of performance, integration and affordability" workshop. Now the system has not accepted my order but also says that I have used the c...

bmdk by Associate II
  • 1208 Views
  • 1 replies
  • 0 kudos