STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Does the Comparator Polarity Selection Work on STM32H7?

I am using an STM32H743ZIT6, and attempting to have COMP1 generate an NVIC interrupt when INP2 is lower than 1/4 Vref_comp. To this end, I set the POLARITY bit in the comparator configuration register to "1", which successfully 'inverts' the "cmp1_ou...

NickFF by Associate II
  • 1978 Views
  • 1 replies
  • 0 kudos

USART - no NACK output

Hello,I am trying to use STM32L476 to interact with a Smartcard.I am using USART1 in "SmartCard with Card Clock" mode.I have the "NACK If Parity Error" enabled.I am having a problem where the USART receiver detects parity error on the line, but does ...

DGabc.1 by Associate III
  • 1973 Views
  • 1 replies
  • 0 kudos

How to see the sent value in UART Data Register?

I send the number 5 via UART to the Data Register, at a speed of 600 bit / s.I watch the Data Register in Keil.The Data Register value is always zero.Is it because the data transfer is very fast?In my case 1/600==0.00166 seconds per bit.I set Breakpo...

_legacyfs_online_stmicro_images_0693W00000dDVEzQAO.png
MMust.5 by Senior II
  • 2826 Views
  • 8 replies
  • 0 kudos

Resolved! How to run my programs in QSPI FLASH?

Hello�?Recently, I was planning to use NUCLEO-L432 to create a smartwatch, but I encountered a fatal problem: running a program using external FLASH can cause the program to freeze.​Because I wanted to use LVGL as a graphical interactive interface, t...

_legacyfs_online_stmicro_images_0693W00000dDUb9QAG.png
noob by Associate II
  • 6662 Views
  • 8 replies
  • 0 kudos

STM32L451 not able to DFU program over USART2

Hello, I am using the STM32CubeProgrammer attempting UART connection to the device, but fails with this error. I would greatly appreciate any guidance or suggestions you may have. See below for additional details about the setup. MCU is STM32L451REYP...

_legacyfs_online_stmicro_images_0693W00000dDL8cQAG.png
AxB by Associate
  • 1321 Views
  • 2 replies
  • 0 kudos

B-L462E-CELL1 module is not responding.

My B-L462E-CELL1 module is not responding, the OLED has gone blank and the TeraTerm Window is also not showing any response. How can this problem be solved?I have a hunch that probably the Nx_TCP_Echo_Client.bin binary file may have got corrupted cau...

AKara.11 by Associate
  • 1117 Views
  • 1 replies
  • 0 kudos