STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F411RC Flash �?역�? 대한 �?�기 �? 256k �?��? �?역�? 대한 사용 가능 �?�유

안녕하세요.현재 STM32F411RC 제품�?� 사용하고 있습니다. 해당 디바�?�스�? 대해 담당 펌웨어 엔지니어가 Flash �?역�?� 256k를 넘겨서 Flash memory �?역으로 선언하여 �?�작�?� 시켰는�?� 정�? �?�작�?� �?�었다고 합니다. 전�? 오프 후 해당 �?역�?� �?�어�?� 쓴 �?��?�터가 잘 �?�어진다고 해서 256k �?��?�?� �?역�? 대해 Flash Memory로 정�?�해서 사용하...

UJang.2 by Associate
  • 3103 Views
  • 1 replies
  • 0 kudos

STM32LO51, I want to achieve lowest possible power in sleep while still being able to wake up using UART at 115200 baud rate

I want to be getting my characters , including the first one from uart at 115200 baud rate and use UART to wake up from sleep, how do I do this ? The sleep mode and low power sleep mode, with all gpios changed to analog no pull and all other peripher...

AV.9 by Associate II
  • 2045 Views
  • 2 replies
  • 0 kudos

Unable to create and save data in SD card

Hello, I'm trying to implement a datalogger using a 32F769IDISCOVERY. I would like to be able to create a .txt file, write information on it and save this file on the SD card available on the board. The problem is, I've tried a lot of things, even fo...

ICard.2 by Associate
  • 1646 Views
  • 2 replies
  • 0 kudos

HRTIM_MCR

please do not be silent, dear inhabitants of the forum. I want to understand what the problem is. I'm trying to put the output into an active state using a master timerHRTIM_SETx1R installed MSTPER       HRTIM_MPER==1000   HRTIM_MCR installed CONT P...

MTS by Associate II
  • 2442 Views
  • 4 replies
  • 0 kudos

Does the Comparator Polarity Selection Work on STM32H7?

I am using an STM32H743ZIT6, and attempting to have COMP1 generate an NVIC interrupt when INP2 is lower than 1/4 Vref_comp. To this end, I set the POLARITY bit in the comparator configuration register to "1", which successfully 'inverts' the "cmp1_ou...

NickFF by Associate II
  • 1960 Views
  • 1 replies
  • 0 kudos

USART - no NACK output

Hello,I am trying to use STM32L476 to interact with a Smartcard.I am using USART1 in "SmartCard with Card Clock" mode.I have the "NACK If Parity Error" enabled.I am having a problem where the USART receiver detects parity error on the line, but does ...

DGabc.1 by Associate III
  • 1966 Views
  • 1 replies
  • 0 kudos

How to see the sent value in UART Data Register?

I send the number 5 via UART to the Data Register, at a speed of 600 bit / s.I watch the Data Register in Keil.The Data Register value is always zero.Is it because the data transfer is very fast?In my case 1/600==0.00166 seconds per bit.I set Breakpo...

_legacyfs_online_stmicro_images_0693W00000dDVEzQAO.png
MMust.5 by Senior II
  • 2809 Views
  • 8 replies
  • 0 kudos