STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Start advertisement without Tx Power type in it

  @remi @remi2 I am using 1.16 full.bin stack, as the peripheral.Issue: some hci commands are disabled in the _full.bin. I can't use other bin. Can I achieve it without a different stack? Thanks a lot for all the helpers!   

muslimah by Associate II
  • 1372 Views
  • 1 replies
  • 0 kudos

Resolved! STM32 I2C pins has slow rise up

Hello, I have this problem with the I2C channel of the STM32F103C8T6 (original), the SDA and SCL signal have very steep rise times, and the slave devices do not recognize the commands. In the image you can see that the SDA has more than 1.5us rise wh...

FAndr.5 by Associate III
  • 8897 Views
  • 7 replies
  • 3 kudos

STM32H7 doesn't run properly after flash erase

Hi guysAfter erasing the flash memory with STM32CubeProgrammer, my STM32H745ZI doesn't run CM4 correctly anymore.I'm experiencing this error:Break at address "0xfffffffe"with no debug information available.Should I need to restore some default config...

Resolved! SysTick registers information for U575 MCU

Hello friends! I have been trying to start the systick timer on my NUCLEO 575 board. But somehow I keep rifling through the user guide, yet cannot find information. Could please anybody let me know where exactly in the guide is the description of how...

Skfir by Senior
  • 2096 Views
  • 2 replies
  • 1 kudos

low power mode in stm32u

Hello,I  am working on low power mode with rtos basically I want to enter in low power mode i,e Sleep mode specifically so with RTOS I know about tickless modedevice STM32U5I want know about is there any other way rather than going into tickless  MOD...

PESHWA by Associate II
  • 937 Views
  • 0 replies
  • 0 kudos

Resolved! LSERDY is not ready when boot after power off in VBAT mode.

I had use VBat with external low frequency OSC for RTC which it's can run fine even reset has occurred. But it's has problem when it was boot from power off with VBat. it's going to TimeOut error while checking LSE state in RCC initial./* Check the L...

Tinnagit by Senior II
  • 6099 Views
  • 7 replies
  • 0 kudos

stm32f407 bootloader using usart

Hi, I am currently working on Stm32F407 Microcontroller and I have need a bootloader code for USART. So kindly I am requesting you to share the code as soon as possible. I have completed my project, but because of bootloader I am not able to finalize...

ssah.1 by Associate
  • 5401 Views
  • 5 replies
  • 0 kudos

Detecting BLE Module disconnection

Hi, I am currently working with an STM32L452 as the master MCU, responsible for controlling a BlueNRG M2SP SoC, which is flashed with DTM_spi.hex.During the course of conducting EMC tests on my device, I encountered an issue with ESD immunity testing...

MAndr.7 by Associate II
  • 1227 Views
  • 0 replies
  • 0 kudos