cancel
Showing results for 
Search instead for 
Did you mean: 

Where single stepping with STM32H7 code works?

LMI2
Lead

Some ARM/STM32H7 CPUs have a problem with single stepping through code. Which CPUs didn't have this problem? I have planned to use STM32H750 because it is now somewhat available, but I could swap.

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
AScha.3
Super User

what problem ? i have a H743 here, at work on H733, H7A3, H723...F767 , F207...

no problem on any of them.

so -- what ?

If you feel a post has answered your question, please click "Accept as Solution".

Read the ARM chip identification.

The ones which were an issue were the STM32F746/756 parts (r0p1)

https://community.st.com/s/question/0D50X0000AnssYLSQY/how-can-i-check-the-revision-of-the-m7-core-without-checking-the-registers

https://community.st.com/s/question/0D50X0000BcRH33SQG/stm32h743-cortexm7-core-revision

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Thank you. Must learn to check the revision