STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ADC values fluctuating

The project I am working on presently need to capture dc voltage with precision of 1mv. I am using STM32f446RE development board. As mentioned in the datasheet STM32F446RE have inbuilt ADC of 12-bit resolution and reference voltage is 3.3v. Thus theo...

PAcha.1 by Associate
  • 4745 Views
  • 1 replies
  • 1 kudos

Resolved! The sequence from the ADC_SQR3 register does not work.

My goal now is to understand how ADC works.I know that with the HAL_ADC_Start_DMA function, I can easily read data from multiple pins.Now I want to set up data transfer from pins in semi-automatic mode, without the HAL_ADC_Start_DMA function.I know h...

png.png
MMust.5 by Senior II
  • 4809 Views
  • 15 replies
  • 3 kudos

STM32G474 WKUP Pin needs to be pulled down?

Hello,I’m using an STM32G474 in standby mode and have found some weird behavior. I know the MCU is entering standby mode as the flag is set upon wake up, however the MCU is still drawing ~120μA in standby. The WKUP pin is floating when not pulled up....

Resolved! GPIO set certain bits without affecting others

BTW, what is the forum to ask general programming questions on STM32 architecture?STM32F103C8TxI have two timer interrupt routines, sharing thevoid HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef* htim)call. Depending on which handle is passed, I pro...

Resolved! Porting STM32H7 Composite-Audio-HID to STM32G4

I am trying to develop a HID and UAC Composite Device with STM32G491.I was proceeding with the implementation with reference to I-CUBE-USBD-Composite, but although it is recognized as a Composite Device from Windows 11, a problem like this occurs and...

Resolved! STM32G491 USB Composite(HID & UAC) problem

I have recently developed a USB Compoite (HID Keyborad & Audio Speaker) device using the STM32G491.I have been able to have it recognized as a Composite Device in the Windows 11 Device Manager, and I have been able to input keys and play PC sound fro...