STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H753 with ADIN1200 LAN driver

I'm trying to interface ADIN1200 LAN driver with STM32H753. CubeMX BSP package supports LWIP library for LAN8742 driver, I see that there are some differences in configuration of both the LAN drivers but not very clear which part in the drivers to be...

AShel.1 by Associate III
  • 1603 Views
  • 1 replies
  • 0 kudos

Resolved! Supply Voltage for Sensors STM32F407VG

I am working on stm32f407vg as the mcu for my mobile robot. I use encoder and limit switch sensors and supply it by 5v from lipo battery (through 5A step down converter). stm32 keep overheating the longer i use it. Is it because i supply the sensors ...

syifnrl by Associate II
  • 5042 Views
  • 8 replies
  • 2 kudos

STM32H753XI MCU with W25Q512 in dual flash mode

Hello,I'm using STM32H753XI MCU with two W25Q512JV(its 64Mb) in dual mode, the nCS and data lines are separate, Clock line is same. I've configured the QUAD SPI in dual flash mode as mentioned in AN4760. I'm trying to read the sectors from first flas...

AShel.1 by Associate III
  • 5661 Views
  • 7 replies
  • 0 kudos

RTE_Device vs CubeMX

I am wondering about the state of mcu configuration options.In the past we have exclusively used RTE_Device (Framework classic) to configure devices and over the years we have built our own libraries on top of this system.Although I like the look of ...

Jvan .19 by Associate II
  • 3240 Views
  • 7 replies
  • 0 kudos

Measuring capacitance using an 8-pin STM32

Hi,I designed a circuit using an 8-pin PIC microcontroller, which I would like to replace by a more advanced model.Being a total STM32 neophite, I wante to know if there is an 8-pin device offering the following features (* means the feature is alrea...

i4004 by Associate
  • 3165 Views
  • 2 replies
  • 0 kudos

Resolved! STM32H743: changes in 480MHz version?

Can someone please point me at a document that identifies any changes in the STM32H743 between the original 400MHz capable version and the latest 480MHz versionThanks

Resolved! ADC Readings Effected by Capacitors?

Hello,  I am new to ST boards, so please bear with me! I am trying to get a vibration reading from a beam using a piezoelectric sensor through an analog pin (ADC reading). I noticed in experiment that the timing of the piezoelectric sensor was not qu...

aab_2-1690703659000.png aab_0-1690703397957.png
aab by Associate
  • 3620 Views
  • 3 replies
  • 1 kudos