STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to adjust Compare Value in HRTIM Basic PWM

Hello,currently I am using the NUCLEO-G474RE and the goal is to output a PWM signal simulating a sinewave. Therefore the duty cycle must continuously be adjusted.My issue is that I seemingly cannot do so.The Timer is configured as Timer D, TD1 output...

Matt1234 by Associate II
  • 4413 Views
  • 3 replies
  • 0 kudos

Modifying linker to keep all ram after soft reset

Hi, everyone. I am using stm32l496 and I my application requires me to keep all data in ram after reset. Now i followed these instructions in this link. https://interrupt.memfault.com/blog/noinit-memory it works, like I expected but the thing is I wa...

HZaib.1 by Associate III
  • 5770 Views
  • 7 replies
  • 3 kudos

HAL Library for Medical device EN62304

Hello Everyone I dont know if its the correct place to ask . We design a medical device where EN62304 calss C is applied . the standart says if we use an 3rd party software ( any library ) should be designed to use for medical devices. What about HAL...

STM32L476 SPI incorrect readings

I am trying to communicate with a spectrometer sensor using SPI protocol. With SPI default settings, I am using both arduino and Stm32L476 nucleo boards. (8Bits, MSB First, CPOL Low, CPHA 1 Edge).I read multiple registers from the sensor using both a...

RSath.1 by Associate II
  • 4055 Views
  • 5 replies
  • 0 kudos

HAL_GPIO_TogglePin() not thread-safe

Posted on May 30, 2018 at 21:31STM32Cube_FW_F7_V1.11.0's HAL_GPIO_TogglePin() appears broken in a multi-threaded environment:void HAL_GPIO_TogglePin(GPIO_TypeDef* GPIOx, uint16_t GPIO_Pin){  /* Check the parameters */  assert_param(IS_GPIO_PIN(GPIO_...

Resolved! How to efficiently save and restore the 32F407 FPU context

STM should really post their code to handle FPU context saving and restoring BECAUSE their clients have been asking for over a decade!!!One user stated "the time for a full FPU state save/restore is quite long. A pair of vpush {s0-31}/vpop {s0-s31} t...

Robmar by Senior III
  • 7032 Views
  • 12 replies
  • 0 kudos