STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USBX and STM32U5 crash

I am unable to make working ThreadX USBX Host example for STM32U5 adopted for Nucleo-U575ZI-Q.All, but the last setup step described in Introduction to USBX section 3.3 complete properly, but when finally HAL_HCD_Start() is called, ThreadX crashes. W...

Screenshot 2023-09-18 113103.png
TDJ by Lead
  • 2763 Views
  • 3 replies
  • 1 kudos

Resolved! CAN register not taking any data - STM32F4

Hey all,I’ve recently encountered an issue with setting up the CAN module on my STM32F4 and hope that someone is able to help me:After buying the SN65HVD230 CAN Board, I tried to set up the MCU so it can communicate with the CAN Bus. For that I solde...

SalomonD_0-1694689943730.png
SalomonD by Associate
  • 2835 Views
  • 2 replies
  • 0 kudos

Resolved! Missing info in reference manual

In the STM32L562 reference manual (RM0438), v7.0, the section 11.6.13 "GPIO register map" is missing the registers MODER and PUPDR (which are documented in the preceding sections).

SZano by Associate III
  • 3439 Views
  • 1 replies
  • 0 kudos

Resolved! Is there a possibility to read the HRTIM timer value ?

Hello,I'm planning to use the STM32G474 to read a pulse width. This width is a delay value in nanoseconds.I'm wondering if there is any possibility to use the High resolution timer (HRTIM) for that operation.I would use the events to trigger a rising...

Sidius by Associate III
  • 8109 Views
  • 9 replies
  • 3 kudos

LPUART DMA on STM32L0

Hello everyone,I'm working on a project where i use 2 STM32 MCU which communicate with each other with LPUART and DMA.My STM32 references : STM32L072CBT6 and STM32L010C6T6I have a problem with this communication with LPUART and DMA. I see that error ...

MLam by Associate III
  • 5477 Views
  • 2 replies
  • 0 kudos

Resolved! SDMMC does not work after power cycle

Hi,I am using STM32H747. I have successfully write&read micro sd card over SDMMC2 peripheral while debugging. But after debugging, when I power cycle or reset the board, I am not able to use sd card. I see FatFS open file failing. The board is arduin...

serhat1 by Associate
  • 3978 Views
  • 1 replies
  • 0 kudos