STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! UART Receive code is not working.

I am using STM32F103C8 MCU and Trying to communicate with Quectel EC200U-CN 4G module and i am not getting data through UART2 Receive pin. Please go through my code and suggest mevoid USART2_IRQHandler(void){ if ((USART2->SR & USART_SR_RXNE) != RESE...

Siva Ram by Associate II
  • 3386 Views
  • 5 replies
  • 1 kudos

PowerSTEP01 example code and programmer user guide

Hi, i m trying to program PowerStep01 with SPI on STM32H7, can anyone kindly advise where to locate sample code and tutoral ? or programmer user guide?  A serach online yield this but error on page and file not found. https://my.st.com/content/my_st_...

Resolved! USB on-the-go high-speed (OTG_HS) - core setup confusion

In RM0456 section 73.4.3 OTG_HS core (p.3279) I found the following statement:"The OTG_HS receives the 60 MHz clock from the reset and clock controller (RCC). This is typically generated in the PLL associated with the HS PHY and enabled in the RCC. T...

TDJ_2-1695126149597.png TDJ_1-1695125909206.png
TDJ by Lead
  • 14275 Views
  • 5 replies
  • 2 kudos

What lead times and deliveries are you seeing?

Sorry to bring up the elephant in the room. I just reviewed the ST Q1 quarterly results from April and was astonished to not find anything related to lead times, shortages, or allocations.My company is in the Musical Instrument space. We work with a ...

AHigg by Associate II
  • 5036 Views
  • 7 replies
  • 0 kudos

Resolved! Unintentional splitting of messages sent via UART using DMA

Hi, I'm having a problem with unintentionally splitting a message I'm trying to send over the UART using DMA . I am using one function to send the message:const uint32_t max_value_of_counter_loop = 100; /* in case systick jams */volatile bool was_u1_...

grados73_0-1695638586953.png grados73_1-1695638653997.png grados73_2-1695638696291.png grados73_5-1695638747552.png
grados73 by Associate II
  • 7199 Views
  • 11 replies
  • 4 kudos

Resolved! STM32F723 FMC SDRAM

Hi there,We use a STM32F723 controller and want to connect two external RAM devices.Now we have to select a RAM that fits to the FMC. What we can't find in the reference manual RM0431 is, if SDRAM-DDR functionality is provided or only SDRAM without D...

CObri.1 by Associate III
  • 2612 Views
  • 2 replies
  • 2 kudos

STM32H563MIY3 release date

Hello,Does anybody know what's the planned production release date for the STM32H563MIY3 WLCSP 125C MCU? I am considering it for a future design.Thanks

danderle by Associate II
  • 1284 Views
  • 1 replies
  • 0 kudos