cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G071K8Ux microcontroller temperature rating availability in the future?

RBein.1
Associate III

I am wondering if STM32G071K8Ux microcontroller will be available with 105 °C temperature rating (STM32G071K8U7) in a near future? There is currently only 85 °C rated part (STM32G071K8U6) available for purchase, but it does not meet the specification of the project that it is to be incorporated. I would greatly appreciate if there is someone here that could provide some useful information regarding this topic or at least direct me to the right place/people.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Uwe Bonnes
Chief

Talk to your FAE. Otherwise a STM32G071KBU3 is available at 3 distributors.

RBein.1
Associate III

STM32G071KBU3 this part offers too much flash memory that unnecessarily increases the price of a microcontroller.