STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H7 Complementary PWM: Issue on CHxN

Hello,I am trying to generate a complementary PWM with a timer in my STM32H723VGTx, I configured channel 1 on timer 1 with the PWM Generation CH1 CH1N mode.I set all the parameters of the base timer and the value for the pulse of PWM, but during the ...

MGian.1 by Associate II
  • 6443 Views
  • 6 replies
  • 0 kudos

Do HRTIM faults respect configured deadtime?

HiAssume that i set up an H-bridge and and control it via the HRTIM block and use the build in deadtime features. I then also enable a couple of faults. The bridges safe state will be to set both lower transistors to be OFF and the two upper once to ...

Detecting Missing Encoder Input

I am using LPTIM1 of an STM32WB55 to read the outputs of a quadrature encoder.If I disconnect either of the two inputs, the timer continues to increment or decrement.Is there any way to stop the counter changing value when one of the in puts is missi...

TWood.4 by Associate III
  • 2303 Views
  • 3 replies
  • 0 kudos

Resolved! I2C read & write operation for LTC4015

 Hi,Currently I am working on a stm32 & LTC4015 based smart charger project. When I followed the data sheet the smbus or i2c read & write operation is given as below:-SMBus WRITE WORD PROTOCOL:-S SLAVE ADDRESS Wr A COMMAND CODE A DATA BYTE LOW A DATA...

Resolved! Battery charger using stm32 & ltc4015

Hi currently I am implementing a smart battery charger using stm32 & ltc4015.But i could not understand how to perfectly configure ltc4015 through i2c protocol.So could you please inform me how to write the i2c sequences to safely charge the battery....

STM32G431 one pulse mode

Hello everyone,I am unable to understand how to get one pulse . Tried methods from online but cannot get any result. I only see a sine pulse from the terminals in oscilloscope.I would like to give a pulse of 15 V and 3A for 50 micro seconds to my 3 p...

Kv.2 by Associate
  • 1344 Views
  • 1 replies
  • 0 kudos

STM32G483 ADC Noise when connected to OPAMP PGA Gain -3

Hello,we use a STM32G483RE for analog sampling of downconverted RF signals. To maximize the signal-to-noise ratio in the digital domain we use one of the OPAMPs in inverting PGA mode with a voltage offset that is fed by a differential to single-ended...

gefa_0-1696582303316.png
gefa by Associate
  • 1727 Views
  • 0 replies
  • 0 kudos

SWV not working with STM32F469I-DISCO

I'm using a 32F469IDISCOVERY board (Cortex-M4). The integrated ST-Link V2-1 has firmware V2J37M27 and is configured as "Debug + Mass storage + VCP Modus" (default). It doesn't look like it has a jumper or solder bridge to connect SWO and I think it's...

AWebe.1 by Associate
  • 3722 Views
  • 2 replies
  • 0 kudos