cancel
Showing results for 
Search instead for 
Did you mean: 

ISM330DHCx Angle Reading Error

Amal Babu_
Associate
Hi , STM Community 
i was using the ISM330DHCx 3D accelerometer and gyroscope Sensor for Angle Measurement purpose.
And decided to try with MOTION_FX libraryA  because i found an example related to this library.
i was able to get the Accelerometer and gyroscope values correctly but why i use the MOTION_FX library functions 
MotionFX_propagate(mfxstate, &data_out, &data_in, &dT)   ,  MotionFX_update(mfxstate, &data_out, &data_in, &dT, NULL) to get the angle data  through data_out.rotation[0] , data_out.rotation[1], data_out.rotation[2]
i was getting almost constant data like
data_out.rotation[0] = 356.23 ,
data_out.rotation[1]  = 7.88 ,
data_out.rotation[2]  = 2.34 
 
how to get the accurate angle from this ISM330DHCx sensor , can anyone suggest any way to read angle from the Sensor using MOTION_FX library or any error in the implementation....
 
Details about my test :
1.Controller used : STM32F103T8U6  64KB
2. used in Custom Board 
3. Verified both acceleration and Gyro Values both are changing correctly
4 platform used CUBE IDE
5 CLOCK used 72 MHz
6 connected using i2c at 400KHz
 
int main(void)
{
  /* USER CODE BEGIN 1 */
 
  /* USER CODE END 1 */
  /* MCU Configuration--------------------------------------------------------*/
  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
  HAL_Init();
 
  /* USER CODE BEGIN Init */
 
  /* USER CODE END Init */
 
  /* Configure the system clock */
  SystemClock_Config();
 
  /* USER CODE BEGIN SysInit */
 
  /* USER CODE END SysInit */
 
  /* Initialize all configured peripherals */
  MX_GPIO_Init();
  MX_CRC_Init();
  /* USER CODE BEGIN 2 */
  BSP_I2C1_Init();
  CUSTOM_MOTION_SENSOR_Init( 0, MOTION_GYRO);
  CUSTOM_MOTION_SENSOR_Init( 0, MOTION_ACCELERO);
 
  CUSTOM_MOTION_SENSOR_SetOutputDataRate(0, MOTION_ACCELERO, (float)ALGO_FREQ);
  CUSTOM_MOTION_SENSOR_SetFullScale(0, MOTION_ACCELERO, 4);
  CUSTOM_MOTION_SENSOR_SetOutputDataRate(0, MOTION_GYRO, (float)ALGO_FREQ);
  CUSTOM_MOTION_SENSOR_SetFullScale(0, MOTION_GYRO, 2000);
 
//  MotionFX_CM0P_initialize(MFX_CM0P_MCU_STM32);
//  MotionFX_CM0P_setOrientation("nwu", "nwu", NULL);
//  MotionFX_CM0P_enable_gbias(MFX_CM0P_ENGINE_ENABLE);
//  MotionFX_CM0P_enable_euler(MFX_CM0P_ENGINE_ENABLE);
//  MotionFX_CM0P_enable_6X(MFX_CM0P_ENGINE_ENABLE);
//  MotionFX_CM0P_enable_9X(MFX_CM0P_ENGINE_DISABLE);
  MotionFX_initialize((MFXState_t *)mfxstate);
 
  MotionFX_getKnobs((MFXState_t *)mfxstate, &ipKnobs);
 
  ipKnobs.acc_orientation[0] = 'n';
  ipKnobs.acc_orientation[1] = 'w';
  ipKnobs.acc_orientation[2] = 'u';
  ipKnobs.gyro_orientation[0] = 'n';
  ipKnobs.gyro_orientation[1] = 'w';
  ipKnobs.gyro_orientation[2] = 'u';
 
  ipKnobs.gbias_acc_th_sc = GBIAS_ACC_TH_SC;
  ipKnobs.gbias_gyro_th_sc = GBIAS_GYRO_TH_SC;
 
  ipKnobs.output_type = MFX_ENGINE_OUTPUT_ENU;
  ipKnobs.LMode = 1;
  ipKnobs.modx = DECIMATION;
//  ipKnobs->acc_orientation[0] = 'n';
//  ipKnobs->acc_orientation[1] = 'w';
//  ipKnobs->acc_orientation[2] = 'u';
//  ipKnobs->gyro_orientation[0] = 'n';
//  ipKnobs->gyro_orientation[1] = 'w';
//  ipKnobs->gyro_orientation[2] = 'u';
//
//  ipKnobs->gbias_acc_th_sc = GBIAS_ACC_TH_SC;
//  ipKnobs->gbias_gyro_th_sc = GBIAS_GYRO_TH_SC;
//
//  ipKnobs->output_type = MFX_ENGINE_OUTPUT_ENU;
//  ipKnobs->LMode = 1;
//  ipKnobs->modx = DECIMATION;
 
  MotionFX_setKnobs(mfxstate, &ipKnobs);
 
  MotionFX_enable_6X(mfxstate, MFX_ENGINE_DISABLE);
  MotionFX_enable_9X(mfxstate, MFX_ENGINE_DISABLE);
 
  MotionFX_enable_6X(mfxstate, MFX_ENGINE_ENABLE);
  MotionFX_enable_9X(mfxstate, MFX_ENGINE_DISABLE);
 
    /* OPTIONAL */
    /* Get library version */
  LibVersionLen = (int)MotionFX_GetLibVersion(LibVersion)
  /* USER CODE END 2 */
 
  /* Infinite loop */
  /* USER CODE BEGIN WHILE */
  while (1)
  {
if( Read_Timer >= 100)
   {
    float dT;
 
  fusion_flag = 0;
 
  CUSTOM_MOTION_SENSOR_GetAxesRaw(0, MOTION_ACCELERO, &accr);
 
  CUSTOM_MOTION_SENSOR_GetAxesRaw(0, MOTION_GYRO, &gyro);
 
  /* Convert angular velocity from [mdps] to [dps] */
  data_in.gyro[0] = (float)gyro.x * FROM_MDPS_TO_DPS;
  data_in.gyro[1] = (float)gyro.y * FROM_MDPS_TO_DPS;
  data_in.gyro[2] = (float)gyro.z * FROM_MDPS_TO_DPS;
 
  /* Convert acceleration from [mg] to [g] */
  data_in.acc[0] = (float)accr.x * FROM_MG_TO_G;
  data_in.acc[1] = (float)accr.y * FROM_MG_TO_G;
  data_in.acc[2] = (float)accr.z * FROM_MG_TO_G;
 
  /* Don't set mag values because we use only acc and gyro */
  data_in.mag[0] = 0.0f;
  data_in.mag[1] = 0.0f;
  data_in.mag[2] = 0.0f;
 
  dT = (float) (CurrentTime/1000.0)- (LastTime);
  LastTime = CurrentTime/1000.0;
  
  MotionFX_propagate(mfxstate, &data_out, &data_in, &dT);
  MotionFX_update(mfxstate, &data_out, &data_in, &dT, NULL);
  }
}
}
 
 
Regards 
Amal
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0