STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Using SDMMC_TRANSFER_MODE_STREAM with SDMMC1 on STMH7

I am using the STMH7A3ZI-Q Nucleo Board together with the WFM200S Silicon Labs WiFi Board.The example project of the WFM200S uses the deprecated SDIO library with an F4 Nucelo ( (https://github.com/SiliconLabs/wfx-fullMAC-tools/tree/wifi_examples_ssv...

_legacyfs_online_stmicro_images_0693W00000bi7yjQAA.png
Hueli.1 by Associate III
  • 2870 Views
  • 3 replies
  • 0 kudos

Integrating XPT2046 With STM32H750

I have used an XTP2046 Library with the STM32H750 Board (Bare metal HAL Without RTOS) Is working and and producing Correct results.But When i use a sample TOUCHGFX Project and only read the XPT2046 Value then I get into following problemsDebugger sho...

ZExpo.1 by Senior
  • 4010 Views
  • 3 replies
  • 0 kudos

Resolved! clock cycles needed for eeprom write

Hello , i am looking to know for STM32L051 how long will it take a byte to be written in to eeprom.while writing eeprom does it have any limitations like UART intteruptions? 

Resolved! No source code available for _udivsi3 on STM32G0

Hi,I'm trying a simple program with a modulo operator on a STM32G031 MCU. Everything works fine during launch. But when using debug, it says "No source code available for _udivsi3() at 0x08000204".I know that the debugger is unable to find the source...

2023-10-19 18_25_38-STM32_Project - Source not found. - STM32CubeIDE.png
Montagny by Associate II
  • 4176 Views
  • 7 replies
  • 4 kudos

RTC Losing time after power restart

Hello all,I am working on RTC of STM32F401RC. I have connected a new CR2032 battery to VBAT.My problem is that when I restart the power I lose time. I have disabled the calendar generation and setting time manually so there is no possibility of time ...

KBhon1_0-1697944232160.png KBhon1_2-1697944416432.png
KBhon.1 by Associate III
  • 11920 Views
  • 15 replies
  • 1 kudos

I2C & SPI not working together (STM32F303K8)

Hi, I am trying to simply output information from an I2C device (DS1307 real time clock) to an SPI screen (ST7789) I have tested the code & libraries for the separate devices and they work but as soon as I try adding any SPI commands to the main.c th...

Linkpad by Associate III
  • 2953 Views
  • 5 replies
  • 2 kudos

hello, USART read doesn't work on nucleo board.

I am using stm32u575zit6q. I set Baud Rate 2500000bit/s.(my equipment is only support 2500000bits)usart write is work successful, but read is not.usart read work only 9600bit/s.How do I use the read to work over 9600baud rate? 

스크린샷 2023-10-23 113055.png
Dinggo by Associate II
  • 2637 Views
  • 5 replies
  • 0 kudos