User Activity

Is there an example code to configure the internal VREFBUF on the STMG474RE (Nuclo-G474RE board). to output for example 2.5V to be used by the ADCs. I do not want to use the external reference on the board.ThanksDavid
In dont see a clear indication of the conversion time for differential mode. Is it the same as for single-ended operation?From DS12288 Rev 6, page 139, tconv : Total conversion time (including the sampling time) in ADC clock periods is given as:ts(cy...
Any help is appreciated.I am using the Nucleo-F303ze board with the STM32F303ze MCU. With development using the STM32CubeIDE version 1.12.1. I have set up 3 differential channels on ADC 1 and 3 on ADC 2 for 3 phase computations, with the scaled volta...
I need to have 2 adcs triggered simultaneously. Since i desire 3 differential inputs per ADC for the Nucleo F303zre board i can use ADC 1 and ADC3 . STM32CuneIDE shows the Timer 20 trigger out event is available for both ADC triggering so i intend to...