User Activity

Hi there.I have been reading UM2576 - GDB Server Usage and am wondering how I can configure STM32 Cube IDE to start a debug session using the --persistant option, as described in the GDB server start-up options section on page 214:-e, --persistantSpe...
Using a STM32G0F06I have a bootloader/application that I am debugging. I am facing a strange problem. Often, I command the app to drop to bootloader (via a software reset). When I execute the software reset code, occasionally the core locks up.Here i...
Scenario is that I am debugging my application using ST-Link V2.The device enters stop mode (with debugging still enabled). If I then add a breakpoint while the device is in stop mode, I immediately trigger a hard fault ISR.This is new behaviour tha...
Update: To get it to work, do a fresh install of the IDE, untick the CDT site in "Available Software Sites" (Help->Install New Software then "Manage"), and then install DevStyle from marketplaceSister issue on the Genuitec forum site: https://www...
I have STM32CubeMonitor v1.4.0 installed on my home computer and work computer.On my home computer, there is an option called "Manage Palette" which allows me to add additional nodes from nodered online resourcesOn my work coputer, there is no such o...
Kudos from