STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Specify option bits in source code file

I am about to release firmware to production and would like to include the proper options bits in the firmware so that production can simply program the .elf file at the same time as updating the option bits.  I realize that there are several option ...

Hello, I want to "over-the-air" update an M7 and H7 via an ESP32 but are getting sync failures and Serial timeouts. It's working with M4.

Hello, sorry if this question is in the wrong topic, first post on the STM community.So i'm working with a solution for updating the firmware on a STM32 M7 microcontroller (NUCLEO-F756ZG). I found a project on Github (ESP32-Musings/OTA_update_STM32_u...

_legacyfs_online_stmicro_images_0693W00000bkm5sQAA.png _legacyfs_online_stmicro_images_0693W00000bkm0eQAA.png
HMoe.1 by Associate
  • 2202 Views
  • 1 replies
  • 0 kudos

STM32L4R9 Octo SPI PSRAM

Hi,We have build a custom board based on the STM32L4R9I-EVAL, On our board we also used PSRAM IS66WVH8M8ALL-100We are facing a problems using this  PSRAM and we saw in the following forum discussions that it's a known issue and that the STM32L4R9 Doe...

YossefZ by Associate
  • 1511 Views
  • 1 replies
  • 0 kudos

Resolved! X-Code Audio Problem

Hi,I am using the Stm32f446RC MCU model for a sound application. I am using the X-Cube Audio library (STM32CubeExpansion_Audio_V1.1.1), which claims to support F4 and F7 versions. I want to control the audio levels using the SVC app, but when I call ...

Bills by Associate II
  • 3414 Views
  • 4 replies
  • 0 kudos

ADC and TIMer callbacks

Hi Can anyone help me understand the difference betweena) writing control loop and obtaining ADC values in HAL_ADC_ConvCpltCallback with ADC ISRsinstead ofb) writing control loop and obtaining ADC values in HAL_TIM_PeriodElapsedCallback using TIMER I...

VidhiPa by Associate II
  • 3741 Views
  • 6 replies
  • 0 kudos

Reduce Bluetooth_LE size

I'm looking to reduce the flash size of my projectI saw that the BLE takes a lot of space.I'm already using the custom_ble_stack_conf.h where I enabled only the SECURE_CONNECTIONS_ENABLEDAre there any other steps I can take to reduce the size?Thanks

vly.1 by Associate
  • 1569 Views
  • 1 replies
  • 0 kudos

STM32 Receive Multiple DMX Universes

Hey there,another question. I can successful output 8 DMX universes received via Artnet using DMA (Mem->Periph). At the same time I want the possibility to receive upto 8 different DMX signals connected to the MCU. Therefore I hooked up the receive l...

PUrsu.1 by Associate II
  • 6061 Views
  • 9 replies
  • 0 kudos