STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 HRTIM BURST DMA CONFIGURATION

Hi all,I am trying to configure burst dma on my board (stm32g474). I have successfully configure the dma for single register, however, when I want to configure dma for more than one register, I failed to do that as it only allow me to fill one addres...

OFN by Associate II
  • 2574 Views
  • 2 replies
  • 0 kudos

STM32G0B1 Options Bytes

Dear, I currently use a STM32G0B1 on a custom board ans all worked fine until now. My firmware change the options bytes at running to disable the dual bank and using and single bank Flash.At the power up, the firmware check the options bytes and chan...

YDann.7 by Associate III
  • 10195 Views
  • 8 replies
  • 0 kudos

Resolved! Problem with I2C Interface on STM32F469I-DISCO

Hello, I am trying to write something on the I2C bus to a digital potineometer using the STM32F469I-DISCO board but I get no result, even no response from the device and its like there is no device connected on the bus. I tried the same potineometer ...

mids400 by Associate III
  • 2944 Views
  • 3 replies
  • 1 kudos

Resolved! How to switch a pin between open drain and ground

Hi, I have a pin labeled "DISABLE_HV" that I want switch between open drain and ground (and vice versa) to switch-off and switch-on a DC-DC converter. How can I implement this functionality in the code using HAL library?

ECiot.1 by Associate II
  • 6279 Views
  • 4 replies
  • 1 kudos

Resolved! LPTimer counts only to 1 if running on LSE

Hi, I'm using on a STM32L4R9 a LPTimer1 in interrupt mode. If i use it with the PCLK1, HSI or LSI as clocksource it works as expected. It counts to the ARR value and then the interrupt occours. If i use the LSE as clocksource the LPTimer seems only t...

Resolved! ISOBUS application

Hi everyone, I checked but I couldn't find anything. Is there any application or demo project for ISOBUS communication on STM32 or demo boards? Thanks,Erdem 

Epamuk by Associate III
  • 5235 Views
  • 1 replies
  • 0 kudos

CAN Errors

Hi All,I have written a baremetal program for CAN Tx and Rx for the board STM32f103C8T6.The normal tx and rx function are working fine , next i have to simulate errors to see how the can system i have written works/performs.I have some ideas but am n...