User Activity

Does the current consumption of the micro stm32L151 in stand by mode with the RTC enabled vary with the supply voltage?From my tests I find that by powering the micro with 3.1 V I have a current consumption of about 4 microA while if I power it with ...
I have problem to compile a simple progragram that use usb virtual com for mcu stm32F042G6Ux , i have create the file from stm32cubemx (.ioc file ) when build it i recive this errorSTM32F042G6UX_PROVA.elf section `._user_heap_stack' will not fit in r...
Hello i  two questions ,1) i use mcu STM32F042T6Y a give the same power  supply 3.3v to pin VDD,VDDA and VDDIO2, is this a problem?(many gpio(i chose the gipo tollerant) input  of mcu work to 5V and i use the usb host of mcu )2) i want use  a externa...
I want use this mcu STM32L052T6Yx  to communicate via usb (virtual port com ) whit pc (whith linux system operativ).THE power supply of mcu is 3.3v, can I problems if i directly connect PA11 PA12 PIN  to the pc usb (common ground)? , moreover  on pin...