STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Missing or unaligned sample in buffer when using ADC and DMA

I am using a STM32F767BITx LQFP208. I have to measure 12 channels. 6 channels measure the voltage and 6 other channels measure the intensity. Samples from voltage and insitensities shall be done as simultaneously as possible.I am using ADC1(voltage) ...

ADC1.PNG ADC2.PNG RMoli3_0-1700488802068.png
RMoli.3 by Associate III
  • 1255 Views
  • 0 replies
  • 0 kudos

NAND FLASH 25N01GV with STM32H725 sector erase failure

Hello everyone, I am trying to use STM32H725 processor with NAND FLASH 25N01GV. The installation seems successful. But sector erase always fails with the same error Status Register(0xC0) = 0x04 (EFAIL - Erase Failure )1. JEDEC ID read successful.W25X...

Ayaki.11 by Associate II
  • 4359 Views
  • 6 replies
  • 0 kudos

STM32G030k8 ADC sequencer set not fully configuarable

Hi I already asked for multi channel ADC in STM32G030K8 PA0,PA2,PA5,PA9,PA11,PA12.while debugging I am getting all ADC values as same if I made one by one its working properly Can any one help how to proceed with that.

meena by Associate III
  • 1668 Views
  • 2 replies
  • 0 kudos

STM32U5A9ZJY6QTR Pixel Resolution support

Hello all,What is the pixel resolution support of STM32U5A9ZJY6QTR MCU.I need support of 1080 x 1920 pixel resolution for max 6'' inch display with both MIPI DSI and RGB888 support.Any possible help. 

Ashu123 by Associate
  • 1984 Views
  • 2 replies
  • 0 kudos

STM32WB55 RDP protection level

Hello I am trying to flash code using openocd(through JTAG) in option byte RDP protection level is set to AA(0) but still openocd throwing error memory is write protected can not write on address 0x8000000. Hardware : STM32WB55 Nucleo boardOpenocd Ve...

DineshB by Associate III
  • 4469 Views
  • 7 replies
  • 0 kudos

Resolved! STM32G431KB Nucleo 32 - USART1 RX help

I'm trying to use USART1 for Async however I cannot send data to the board. I'm using an FTDI USB-UART converter cable to test, the Nucleo is sending correct data my PC data no problem.I can prove my code and terminal program on the PC works 2 way wi...

LiamRDS by Associate
  • 3216 Views
  • 4 replies
  • 1 kudos