STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H7 DFU jump to application doesn't work

Controller: STM32H743ZIT6Custom BoardSTM32CubeProgrammer, STM32CubeIDEHi, since a few months we have an issue with flashing our Microcontroller application.We are using automatic firmware flashing over DFU-Util on a Linux based system, which is conne...

PStoc.3 by Associate II
  • 3323 Views
  • 4 replies
  • 1 kudos

Resolved! Delay with timers(Non blocking delay)

Hi,I need  microsec/millisec delay  in my project but I don't want to effect the process flow.I am using STM32G4.I am using timer for microseconds delay below is the function.void delay_us (uint16_t us){__HAL_TIM_SET_COUNTER(&htim1,0); // set the cou...

Resolved! RNG does not work after waking up from the stop mode

Hello,My MCU is STM32L053R8I use freeRTOS project generated by CubeMX.The problem is happening only  when I enable tickless sleep. I get only one correct reading, which is probably generated right after MX_RNG_Init. Then after the sleep, I always get...

Evgeny M by Associate II
  • 2869 Views
  • 2 replies
  • 2 kudos

STM32H723ZG AZURE RTOS - Hard Fault Error Regarding

As we are using STM32H723ZG-CT6 for our Medical project. We are using STM's Complement to STMH7 series - Azure RTOS for our project. We were runs totally 8 threads, during the running time of threads Hard fault error is coming and our controller stop...

Screenshot 2023-11-27 190422.png
rkuma.21 by Associate III
  • 2371 Views
  • 2 replies
  • 1 kudos

Uart to int conversion

Hi im hoping someone can help me, honestly it might be a easy thing to do, however i have been cracking my brain around this and can't seem to get it to work. uint8_t Rx_data[6] = {0}; HAL_UART_Receive(&huart1, Rx_data, 6, 1000);printf("%s\n", Rx_dat...

VYada.3 by Associate II
  • 4366 Views
  • 4 replies
  • 0 kudos

AN4457-emulated-uart

안녕.HAL_UART_Emul_Receive_DMA 및 HAL_UART_Emul_Transmit_DMA를 사용하고 있습니다.1Byte R/W를 시도 중입니다. stm32 go Error_Handler();코드를 어떻게 변경해야 하나요? 감사합니다. 

JLee.21 by Associate II
  • 1884 Views
  • 2 replies
  • 0 kudos

Resolved! STM32H563 Flash Erase Program sample fails in Keil

I create sample code for FLASH Erase Program on both mdk arm and stm32cubeide. Using the sample hardware(stm32h563ZITx develop board), the sample code runs correctly on stm32cubeide, but will enter Error hander when doing Flash operation in keil debu...

Ehow by Associate II
  • 8037 Views
  • 6 replies
  • 1 kudos

ADC input disturbed by PWM

I'm having an issue with my STM32F303RE. I'm using CubeMX to initialize ADC1_IN1 as single ended on PA0, and PWM generation on TIM2_CH1 on PA15. Unfortunately, PA0 will OUTPUT a voltage roughly proportional with the duty cycle of the PWM on PA15, i.e...

kristblo by Associate II
  • 5929 Views
  • 12 replies
  • 1 kudos

Resolved! Enabling USB Device CDC on Nucleo F303ZE

I have a Nucleo F303ZE and enabled USB Device middleware along with the USB 'Device FS' Connectivity.  I also configured the CDC_SET_LINE_CODING and CDC_GET_LINE_CODING  functions in USB_DEVICE/App/usbd_cdc_if.c I connect a USB cable to the STLink co...

LMorr.3 by Senior II
  • 3056 Views
  • 6 replies
  • 3 kudos