STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! DMA RX complete interrupt sometimes not called in STM32L4

Hi everyone, I've done these steps before on STM32F0, STM32F1 and STM32F4 microcontrollers to detect when a circular DMA buffer for UART "wraps" (The counter finishes with the array and starts from the beginning again) with complete successActivated ...

IJoe.1 by Associate II
  • 2422 Views
  • 1 replies
  • 0 kudos

Resolved! Timer update generation delay

Hello,I am verifying timer functionality on an STM32F303K8 Nucleo development board. After generating an update event, the counter register does not update immediately - in downcounting mode, it takes several nops for the counter to read the same as ...

bsakas by Associate II
  • 2516 Views
  • 2 replies
  • 0 kudos

How to dynamically reassign the pin?

Originally, I configured PB6 to work with OneWire using DMA! However, after some time, I need to use the same pin for operating an LED!Below are the steps to reset the pin settings to default.1. Stopping all processes associated with using DMA on pin...

DK.7 by Senior
  • 1567 Views
  • 2 replies
  • 1 kudos

Differences between Revisions of STM32F205

Hello,There are 8 revisions of the STM32F205: 'Y', 'X', '1', 'V', '2', '3', '4' and '5'.The silicon errata shows the status of support for all revisions, with no mention of individual revisions.Does this mean that all revisions are the same?Is it cor...

rev.jpg
YYama.4 by Associate
  • 2571 Views
  • 3 replies
  • 3 kudos

Resolved! Flash erase blocking GPIO updates

I am testing doing flash erase while running code from internal SRAM on a STM32F072B Discovery Board. Having initializing everything with code running in flash, I call a function where itself and all its dependencies exist in RAM. I've verified this ...

link87 by Associate II
  • 15181 Views
  • 11 replies
  • 6 kudos

Receving a string from terminal via UART

Hey, I would like to a string from terminal via UART in order to complete a challange given by Digi-Key YouTube channel in FreeRTOS tutorial playlist. Anyway, I want to take the whole string given by user in terminal, but I couldn't so far. I tried  ...

Resolved! Cannot read ID from external flash (OSPI1) on STM32H735-DK

Hello all, I was trying to follow the example in MOOC - STM32H72x/3x hands-on workshop - 6 Code execution from external FLASHI have configured the OSPI as per the board requirements in CubeMX. But the `OSPI_Init()` function fails while trying to read...

NRedd.2 by Senior
  • 3896 Views
  • 4 replies
  • 0 kudos

Resolved! Can not set up PWM for a different Pin than PA5

Hey,after trying to setup a different PIN for example: PC0 for PWM I just can not get it to work.But this sample code works only for PA5:  #include "stm32f3xx.h" int main(void) { RCC->AHBENR |= RCC_AHBENR_GPIOAEN; RCC->APB1ENR |= RCC_APB1ENR_TIM2E...