STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! USB CDC device stuck

Hi All,Here is the situation:Device: STM32G0B1CET6N - connected to PC with USB. USB CDC stack is running inside MCU.PC:Win10 Pro 64-bit, COM-port is recognized, Teraterm is running and both in and out data directions are working OK when the Teraterm ...

Rise by Associate II
  • 5665 Views
  • 6 replies
  • 3 kudos

Resolved! Does stm32H563 support 2wire USB

I'm using STM32H563, and just use USB_DM USB_DP for usb connect and without connect UCPD_CC1 UCPD_CC2, can it work for USB type-a connect and worked as host for msc storage. Thank you.

runbaby by Associate
  • 1127 Views
  • 1 replies
  • 1 kudos

Resolved! STM32G030 microsecond delay

Hello guys. I am working with STM32G030 MCU for delay in millisecond HAL_Delay();is working fine.but I want to do a delay in microseconds so will you please guide how I can do this? I followed this tutorial but not getting desired result.https://cont...

sandeep3 by Associate II
  • 18663 Views
  • 3 replies
  • 4 kudos

STM32F411E-DISCO cannot send Can data via I2C interrupt

 Hello, I am trying to take imu and encoder data in Stm32 and transfer it from can network via mcp2515. When I try to transfer data in the encoder, it works without any problems when I apply CANSPI_Transmit in the callback function.However, CANSPI_Tr...

sheqom by Associate III
  • 4998 Views
  • 4 replies
  • 0 kudos

Resolved! how to get usb status

HELLOI am working with Xmodem  file transferring vai usb  I want to know how i get know about USB status like  Ready or not how we get in UART  while (!(HAL_UART_GetState(&huart4) == HAL_UART_STATE_READY) && wTimeout) {wTimeout--;}if (HAL_UART_GetSta...

PESHWA by Associate II
  • 1664 Views
  • 2 replies
  • 0 kudos

Resolved! NUCLEO-F722ZE Clock and MO2 issues

I'm attempting to set the clock to PLL on the board mentioned and view the output on MCO2. This is some of the defines I use  #define REG_SET_BIT(reg,pos) ((reg) |= (1U << (pos))) #define REG_CLR_BIT(reg,pos) ((reg) &= ~(1U << (pos))) ...

MHank.1 by Associate III
  • 2105 Views
  • 3 replies
  • 0 kudos

Problem setup in Logic Analyzer in keil

Posted on February 11, 2016 at 17:04I use STM32f103RCT6 to blinking led in pin A8 with 1 second delay, and i try to use logic analyzer to see whether it's right. However, when i setup in ''Current Logic Analyzer Signal'', i write PA.8 in it and it s...

0690X00000605LcQAI.png

I can't write code to my own STM board

Hello, friends. This is my season project. I am trying to send data and control servo to my stm32f103rbt6 MPU using HC-05. I made this board but I can't write code to my own MPU. Also I can start my bluetooth module in AT mode but I can't find HC-05 ...

Ekran görüntüsü 2023-12-15 020417.png WhatsApp Görsel 2023-12-15 saat 01.55.52_01d2e681.jpg WhatsApp Görsel 2023-12-15 saat 01.55.54_2a6b6838.jpg 1.png
bbayrm by Associate
  • 2501 Views
  • 4 replies
  • 1 kudos

STM32H7 - UART DMA working only in debug mode

dear all, my STM32H7 based project implements three DMA streams, one for a SAI peripheral, a second one for the ADCs and the third one for UART comm.static void MX_DMA_Init(void) { /* DMA controller clock enable */ __HAL_RCC_DMA1_CLK_ENABLE(); /* DMA...

Mdi c by Associate III
  • 2490 Views
  • 3 replies
  • 1 kudos