STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32G473 BFB2 Not Working

BFB2 Set, but never enter Bank2 program.Boot0 = 0Boot1 = 1I can run the 2 programs from cubeide in there respective locations and ISR work when BFB2 is set for the BANK I am debugging in. However I never enter BANK2 program on resetting/powercycling ...

kip18 by Associate II
  • 2600 Views
  • 5 replies
  • 0 kudos

Jum to Bootloader from application without PIN.

Hi,I am developing a bootloader, I would like to flash the STM32 using another MCU using USART.My question is, If it possible to enter into bootloader mode without using external pins? I would like to enter just by software, is that possible?I see th...

mtapia by Associate
  • 932 Views
  • 3 replies
  • 0 kudos

How to enable Fast Mode Plus(Fm+) for I2C on STM32L496?

I'm trying to configure the I2C to run at 1Mhz(Fm+) on STM32L496. As per the RM0351, it does support fast mode plus mode. I tried generating the code from STM32Cube IDE and check the SCL pin of logic analyzer. However, I see 400 khz I2C clock frequen...

0693W00000NqrMkQAJ.png
ANath.1 by Associate III
  • 4316 Views
  • 5 replies
  • 0 kudos

Resolved! STM32H5 DSP support

I'm trying to use CMSIS DSP on a STM32H563, but I do not get the expected results.In X-CUBE-ALGOBUILD.1.3.0, when I select DSP Library  in STM32CubeMX, the installed arm_math.h does not list Cortex-M33 support: #error "Define according the used Corte...

PieterG by Associate III
  • 1954 Views
  • 3 replies
  • 2 kudos

Resolved! Issue receiving CAN Frames

Hello ST community,   I am currently programming an ECU system, using f446re nucleo board. Right now i am trying to communicate with BMS using CAN communication. So far, everything has been set: CAN Initialization and start, sending works properly. T...

Erwan03 by Associate III
  • 3153 Views
  • 11 replies
  • 1 kudos

STM32F4 DMA Address Update penalty with double buffering

So the background is essentially this - I am trying to use one of the streams of STM32F4 DMA2 in circular, DBM mode.The DMA stream is being used to move data out of the SPI DR register at regular intervals, as soon as data becomes available at SPI RX...

ribdp_0-1716293619991.png
ribdp by Associate II
  • 1139 Views
  • 4 replies
  • 0 kudos

STUSB4500

Hello,i am trying to configure the STUSB4500 on a Eval-SCs001v1 with a F446RE Nucleo board using I2C connection. from my understanding am i unable to use the GUI to make the NVM files because that wont reconize my Nucleo board. Also the example proje...

ThomasDisSensors_0-1718193967638.png ThomasDisSensors_1-1718196101906.png

Resolved! STM32H7 ADC DMA don't run with LWIP and RTOS

Hello everyone,I have to use the ADC 16b converter with DMA which does not work if DCache is enabled but, to use LWIP and RTOS it is necessary that DCache is enabled.Does anyone know how to fix the problem?Thank you in advance

Stefano1 by Associate II
  • 1020 Views
  • 2 replies
  • 0 kudos