STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! I CAN'T FIND THE STM32L053R8 S MEMORY MAPPING

In the datasheet of the stm32l053x in the section of "Memory mapping" it says "Refer to the product line reference manual for details on the memory mapping as well as the boundary addresses for all peripherals."I looked at the reference manual and di...

ALMAAROUF by Associate II
  • 2119 Views
  • 3 replies
  • 1 kudos

System crashing HTTP execution with GSM module

Well, I'm developing a system for reading sensors and sending them to a server.I'm using a GSM LTE module to do this sending. At first it worked well, but after a while the system stopped sending messages to the server.We can see this clearly in the ...

Capturasdfasdfasd8ar.PNG Capturasdfasdfasdar.PNG sssad.PNG

H747I-Disco expanding on an example file

hello forumI've been playing with a H747I-Discovery board, and I want to add some more functionality to a combination of example codes - activating one of the i2c.the example itself doesn't include an .IOC file.As I see it I have two options:1.Start ...