STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1547 Views
  • 0 replies
  • 2 kudos

Resolved! How to understand the STM32N6 using STM32Cubemx

I am using a STM32N6570-DK board and I can't understand how to configurate the FSBL, Application, and the External memory stuff in Cubemx. Can anyone describe how to use and configurate these three options?

Z-YF by Associate III
  • 2130 Views
  • 2 replies
  • 1 kudos

Generating CMake project using NetXDuo is broken

When generating a CMake project using NetXDuo with lan8742 as phy driver and DHCP Client enabled, the necessary includes for the lan8742 bsp component and the dhcp client addon are missing from the CMake build configuration.However when using the STM...

mo_krauti by Associate III
  • 1295 Views
  • 3 replies
  • 1 kudos

STM32CubeMX Ethernet Rx Buffer Over Allocation

Using STM32CubeMX 6.14.0 with H7 package 1.12.1.When Ethernet is set up with number of RX descriptors set to 16, the default LWIP ethernet driver rx buffer pool overflows. This is caused by during startup, HAL_ETH_Start_IT calls ETH_UpdateDescriptor....

ADunc1_1-1744241328464.png ADunc1_2-1744241358572.png
ADunc.1 by Senior II
  • 1523 Views
  • 2 replies
  • 1 kudos

Resolved! Threadx support missing for F4 and F7?

Hi guysI can't find threadx support for F4, F7 and H7, it's only available for C0 series. According to this post, and my google. It should support most stm32 MCUs. What can I do to enable threadx support for these MCUs? 

User_bug13_0-1743374497493.png

Resolved! STM32WL pin context assignment missing

 Hi ST-Community, I have a problem with my STM32CubeMX: The pin context assignment for STM32WL55JCI7 is missing. Does anyone have the same problem and know how to fix it? (No generated code for GPIOs) Many thanks in advance for your support! Kind reg...

PhilKnufWT_2-1744197960725.png PhilKnufWT_1-1744197927597.png