Skip to main content
Semer CHERNI
ST Employee
April 14, 2025
Question

STM32CubeMX 6.14.1 released

We are pleased to announce that the minor version 6.14.1 of STM32CubeMX is available.

What is new in 6.14.1:

  • SAI settings not displayed in the configuration tab of STM32H7Bxxx devices:
    • After upgrading to STM32CubeMX 6.14.0, the SAI tab configuration is lost.
  • DCMI building problems in STM32N6 projects:
    • DCMI initialization instructions are not generated for both secure and nonsecure domains.
  • Failure in generating the initialization instructions for projects using the DCMIPP feature in CSI mode.
  • ULPI_Clock initialization issues for STM32F7 projects using the USB_OTG_HS feature:
    • STM32CubeMX generated code omits the ULPI_Clock initialization or adds it when it is not needed.
  • STM32WBA63xx project generation issues:
    • STM32_WPAN advertising menu elements not updated correctly.
    • Inaccurate warnings about non configured peripherals.
    • IOC files failing to reopen, reverting to the home screen.
  • stdio.h inclusion error for STM32U5 projects:
    • A preprocessor error occurs in the compilation of STM32U5 projects because the #include statements in main.h are not properly delimited by new lines (more precisely, the inclusion of stdio.h in main.h is done with no line ending).
  • Failure to create projects that activate the SDMMC feature with a basic application structure.
  • CMake and makefile issues with STM32WB series projects when configuring the STM32_WPAN middleware:
    • STM32CubeMX incorrectly removes the STM32_WPAN middleware settings from CMake and makefile configuration files during subsequent code generations, which leads to compilation errors.
  • Memory management issue with STM32H5 projects when Arm® TrustZone®(a) is enabled

Main fixed issues in 6.14.1:

Refer to the STM32 microcontroller wiki at:
https://wiki.st.com/stm32mcu/wiki/Category:STM32CubeMX_errata

Known problems and limitations in 6.14.1:

Refer to the STM32 microcontroller wiki at:

https://wiki.st.com/stm32mcu/wiki/Category:STM32CubeMX_errata

How to get STM32CubeMX 6.14.1:

  • Under this link
  • Or update your current installation of STM32CubeMX using: Help > Check for Updates

 

This topic has been closed for replies.