Hi all,I'm developping an application under system workbench for STM32. The compilation works fine, but when it comes to the Linker I get the following output : 16:08:46 **** Incremental Build of configuration Release for project Firmware **** make a...
Hi,Recently I got nucleo board with mentioned MCU. I've had numerous troubles with generating properly project and finding any sources how to flash the device so few things:Is CubeMX generating code properly for dual core for any toolchain? I've trie...
I installed STM32CUBEMX version 6.1.1 for the project of STM32L5. As I edited Project, I couldn't change Toolchain/IDE to SW4STM32.As below image, I could select only EWARM, MDK-ARM, and STM32CubeIDE.When I make the code through other toolchain...
I am on macOS 10.13.6 High Sierra. I own a NUCLEO-F446RE board.I am trying to build a simple test project with SystemWorkbench, i.e. SW4STM32.I open STM32CubeMX, I select my NUCLEO board, I select SW4STM32 as Toolchain/IDE, I press "generate code" an...
I noticed that my .text section gets mapped at one of two different addresses depending on my build. In one instance the hex file had a small (8 byte) gap in it which was causing some issues with some hex file parsing that I do. I've since worked aro...
Hi !After generating code for the tool chain SW4STM32 the Eclipse project setting "exclude from build" for files or folders is reset:used software versions:STM32CubeMx 5.6.1Eclipse 2020-06 (4.16.0)Eclipse AC6 plugins: Bug or feature ?Best regards, Mi...
Hello, i have got problem with basic project form STM32CubeMX. Help please.This is my project https://drive.google.com/file/d/1nJh5805ZFjzibTgeT_i-kSdNzgrmXk0_/view?usp=sharing for STM32CubeMXI write in SW4STM32 main.c:* USER CODE BEGIN Includes */ #...