STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1574 Views
  • 0 replies
  • 2 kudos

port A pins not correctly configured for input capture

I've discovered that when I configure the TIM2 timer to ‘input Capture direct mode’ for any port A input pin it doesn’t add the necessary line in  HAL_TIM_Base_MspInit() to configure the pin to alternate mode, namely the following line is missing in ...

kswST by Associate II
  • 999 Views
  • 2 replies
  • 1 kudos

Can't use RTT with CMake project

I tried to use cmake with CubeMx but I cant make RTT works.Error:multiple definition of `_write_r'; /usr/lib/gcc/arm-none-eabi/13.2.0/../../../../arm-none-eabi/lib/thumb/v7-m/nofp/libc_nano.a(libc_a-writer.o):/build/arm-none-eabi-newlib/src/build-nan...

Hyderman by Associate II
  • 6715 Views
  • 9 replies
  • 1 kudos

CubeMX octospi code generation

Hi everyone,I noticed that CubeMX 6.14.0 ignores the octospi parameter settings. I created a new project for the NucleoU5A5 board, configured Octospi1 with a clock prescaler of 99. I notice the following behaviorGenerated code (CubeIDE) has a prescal...

tzijnge by Associate II
  • 1241 Views
  • 3 replies
  • 0 kudos

Resolved! USBX Add Custom Class

MCU:STM32U585xxEnv:ThreadX + USBX + FileXI want to use USBX add my own class type, but I'm already have 3 classes, HID, MSC and CDC ACM, it means 4 classes after added my own.In file (ux_device_descriptors.h) have a define (USBD_MAX_SUPPORTED_CLASS  ...

Jason927 by Associate III
  • 1213 Views
  • 1 replies
  • 0 kudos

Custom User Code Sections

In many cases, especially for middleware, it may be necessary to extend the code generated by CubeMX.Since not all files have sections that are untouched by the code generator or some places inside a file are missing those user code sections, I'm oft...

dmocom by Associate II
  • 6798 Views
  • 7 replies
  • 9 kudos

Resolved! Ethernet PHY type resets itself

Hi,A small but annoying bug with STM32CubeMX 6.14.0 with H7 package 1.12.1.  Every time I change anything in the LWIP general settings (e.g. DHCP enable/disable), the PHY setting changes by itself from USER_PHY to undefined. This is a nuisance as if ...

ADunc1_0-1743728005237.png
ADunc.1 by Senior II
  • 1526 Views
  • 1 replies
  • 1 kudos